ConnectionFinderBuilder Class¶
-
class
NXOpen.Weld.
ConnectionFinderBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a builder to display, manage, delete, and allow the user to reparent face information for the weld objects.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Filter | Returns or sets the filter values to contol Save All processing. |
ListFeatureSet | Returns or sets the option to list the search results according to the feature sets that the specified weld point belongs to. |
ReassignEdge | Returns the edges to use when the reassign button is invoked. |
ReassignFace | Returns the faces to use when the reassign button is invoked. |
Tag | Returns the Tag for this object. |
UpdateCoordinateSystem | Returns or sets the option to update the coordinate system for the node from the obtained reconnection when saved. |
Methods¶
Method | Description |
---|---|
CenterNode | Adjusts the display of the part and fits the selected weld points in the center of the graphics window. |
ClearAllTree | Clears the tree list and allows you to perform another search. |
ClearMarking | Unmarks (removes save or delete mark) the weld feature from processing. |
DeleteNode | Deletes the connected part information from the results. |
GetEdgeNodeCollector | Get the edge collector for a specific weld object and index. |
GetFaceNodeCollector | Get the face collector for a specific weld object and index. |
GetFaces | Get the face collectors for the given feature set or point depending on the NXOpen.Weld.ConnectionFinderBuilder.ListFeatureSet`() . |
IsEdgeNodeEmpty | Identify if the edge collector for a specific weld object and index has edges assigned to it. |
IsFaceNodeEmpty | Identify if the face collector for a specific weld object and index has faces assigned to it. |
ReassignEdgeNode | Reassign the edges from the Reassign Edge collector to the specified node. |
ReassignFaceNode | Reassign the faces from the Reassign Face collector to the specified node. |
ReorderAfterEdgeNode | Reorders a selected edge by putting it after the specified edge. |
ReorderAfterFaceNode | Reorders a selected face by putting it after the specified face. |
ReorderBeforeEdgeNode | Reorders a selected edge by putting it before the specified edge. |
ReorderBeforeFaceNode | Reorders a selected face by putting it before the specified face. |
RequiredFaceNode | Identify if the face node is required (true) or optional (false). |
SaveAllTree | Identify all the connected part information as saved so the commit will save the information. |
SaveNode | Identify the connected part information as saved so commit will save the information. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConnectionFinderBuilderFilterTypes Enumeration | Filter values to control Save All processing. |
Property Detail¶
Filter¶
-
ConnectionFinderBuilder.
Filter
¶ Returns or sets the filter values to contol Save All processing.
-------------------------------------
Getter Method
Signature
Filter
Returns: Return type: NXOpen.Weld.ConnectionFinderBuilderFilterTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Filter
Parameters: filter ( NXOpen.Weld.ConnectionFinderBuilderFilterTypes
) –New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
ListFeatureSet¶
-
ConnectionFinderBuilder.
ListFeatureSet
¶ Returns or sets the option to list the search results according to the feature sets that the specified weld point belongs to.
-------------------------------------
Getter Method
Signature
ListFeatureSet
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ListFeatureSet
Parameters: listFeatureSet (bool) – New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
ReassignEdge¶
-
ConnectionFinderBuilder.
ReassignEdge
¶ Returns the edges to use when the reassign button is invoked.
-------------------------------------
Getter Method
Signature
ReassignEdge
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
ReassignFace¶
-
ConnectionFinderBuilder.
ReassignFace
¶ Returns the faces to use when the reassign button is invoked.
-------------------------------------
Getter Method
Signature
ReassignFace
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
UpdateCoordinateSystem¶
-
ConnectionFinderBuilder.
UpdateCoordinateSystem
¶ Returns or sets the option to update the coordinate system for the node from the obtained reconnection when saved.
-------------------------------------
Getter Method
Signature
UpdateCoordinateSystem
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpdateCoordinateSystem
Parameters: updateCoordinateSystem (bool) – New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
Method Detail¶
CenterNode¶
-
ConnectionFinderBuilder.
CenterNode
¶ Adjusts the display of the part and fits the selected weld points in the center of the graphics window.
Signature
CenterNode(nodeTag)
Parameters: nodeTag ( NXOpen.NXObject
) – Weld Feature.New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
ClearAllTree¶
-
ConnectionFinderBuilder.
ClearAllTree
¶ Clears the tree list and allows you to perform another search.
Signature
ClearAllTree()
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
ClearMarking¶
-
ConnectionFinderBuilder.
ClearMarking
¶ Unmarks (removes save or delete mark) the weld feature from processing.
Signature
ClearMarking(nodeTag)
Parameters: nodeTag ( NXOpen.NXObject
) – Weld Feature.New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
DeleteNode¶
-
ConnectionFinderBuilder.
DeleteNode
¶ Deletes the connected part information from the results.
Signature
DeleteNode(nodeTag)
Parameters: nodeTag ( NXOpen.NXObject
) – Weld FeatureNew in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
GetEdgeNodeCollector¶
-
ConnectionFinderBuilder.
GetEdgeNodeCollector
¶ Get the edge collector for a specific weld object and index.
This is useful when the edge node for the object is empty and you need to populate it. Search will be limited by the list feature set setting.
Signature
GetEdgeNodeCollector(weldObject, edgeNodeIndex)
Parameters: - weldObject (
NXOpen.NXObject
) – Specific weld feature set or point to search for. - edgeNodeIndex (int) – Specific position index to look for in the weld object.
Returns: Can return None if not found.
Return type: New in version NX9.0.0.
License requirements: None.
- weldObject (
GetFaceNodeCollector¶
-
ConnectionFinderBuilder.
GetFaceNodeCollector
¶ Get the face collector for a specific weld object and index.
This is useful when the face node for the object is empty and you need to populate it. Search will be limited by the list feature set setting.
Signature
GetFaceNodeCollector(weldObject, faceNodeIndex)
Parameters: - weldObject (
NXOpen.NXObject
) – Specific weld feature set or point to search for. - faceNodeIndex (int) – Specific position index to look for in the weld object.
Returns: Can return None if not found.
Return type: New in version NX9.0.0.
License requirements: None.
- weldObject (
GetFaces¶
-
ConnectionFinderBuilder.
GetFaces
¶ Get the face collectors for the given feature set or point depending on the
NXOpen.Weld.ConnectionFinderBuilder.ListFeatureSet`()
.Signature
GetFaces(weldObject)
Parameters: weldObject ( NXOpen.NXObject
) – Specific weld feature set or point to search for.Returns: Face Collectors. Return type: list of NXOpen.ScCollector
New in version NX10.0.2.
License requirements: None.
IsEdgeNodeEmpty¶
-
ConnectionFinderBuilder.
IsEdgeNodeEmpty
¶ Identify if the edge collector for a specific weld object and index has edges assigned to it.
Search will be limited by the list feature set setting. An error will be returned if the edge node cannot be found or the collector is missing.
Signature
IsEdgeNodeEmpty(weldObject, edgeNodeIndex)
Parameters: - weldObject (
NXOpen.NXObject
) – Specific weld feature set or point to search for. - edgeNodeIndex (int) – Specific position index to look for in the weld object.
Returns: Return type: bool
New in version NX9.0.0.
License requirements: None.
- weldObject (
IsFaceNodeEmpty¶
-
ConnectionFinderBuilder.
IsFaceNodeEmpty
¶ Identify if the face collector for a specific weld object and index has faces assigned to it.
Search will be limited by the list feature set setting. An error will be returned if the face node cannot be found or the collector is missing.
Signature
IsFaceNodeEmpty(weldObject, faceNodeIndex)
Parameters: - weldObject (
NXOpen.NXObject
) – Specific weld feature set or point to search for. - faceNodeIndex (int) – Specific position index to look for in the weld object.
Returns: Return type: bool
New in version NX9.0.0.
License requirements: None.
- weldObject (
ReassignEdgeNode¶
-
ConnectionFinderBuilder.
ReassignEdgeNode
¶ Reassign the edges from the Reassign Edge collector to the specified node.
Signature
ReassignEdgeNode(ownerTag, nodeTag)
Parameters: - ownerTag (
NXOpen.NXObject
) – Weld Feature Set or Feature Point. - nodeTag (
NXOpen.NXObject
) – Edge, or collector, identify which edges to modify in set or point.
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
- ownerTag (
ReassignFaceNode¶
-
ConnectionFinderBuilder.
ReassignFaceNode
¶ Reassign the faces from the Reassign Face collector to the specified node.
Signature
ReassignFaceNode(ownerTag, nodeTag)
Parameters: - ownerTag (
NXOpen.NXObject
) – Weld Feature Set or Feature Point. - nodeTag (
NXOpen.NXObject
) – Face, or collector, identify which faces to modify in set or point.
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
- ownerTag (
ReorderAfterEdgeNode¶
-
ConnectionFinderBuilder.
ReorderAfterEdgeNode
¶ Reorders a selected edge by putting it after the specified edge.
Indices start at 0 for the 1st element.
Signature
ReorderAfterEdgeNode(parentTag, edgeSetIndexToMove, edgeSetIndexToReoderAfter)
Parameters: - parentTag (
NXOpen.NXObject
) – Parent Weld Feature. - edgeSetIndexToMove (int) – Index of the edge set to reorder
- edgeSetIndexToReoderAfter (int) – Index of the edge set to reposition after
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
- parentTag (
ReorderAfterFaceNode¶
-
ConnectionFinderBuilder.
ReorderAfterFaceNode
¶ Reorders a selected face by putting it after the specified face.
Indices start at 0 for the 1st element.
Signature
ReorderAfterFaceNode(parentTag, faceSetIndexToMove, faceSetIndexToReoderAfter)
Parameters: - parentTag (
NXOpen.NXObject
) – Parent Weld Feature. - faceSetIndexToMove (int) – Index of the face set to reorder
- faceSetIndexToReoderAfter (int) – Index of the face set to reposition after
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
- parentTag (
ReorderBeforeEdgeNode¶
-
ConnectionFinderBuilder.
ReorderBeforeEdgeNode
¶ Reorders a selected edge by putting it before the specified edge.
Indices start at 0 for the 1st element.
Signature
ReorderBeforeEdgeNode(parentTag, edgeSetIndexToMove, edgeSetIndexToReoderBefore)
Parameters: - parentTag (
NXOpen.NXObject
) – Parent Weld Feature. - edgeSetIndexToMove (int) – Index of the edge set to reorder
- edgeSetIndexToReoderBefore (int) – Index of the edge set to reposition before
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
- parentTag (
ReorderBeforeFaceNode¶
-
ConnectionFinderBuilder.
ReorderBeforeFaceNode
¶ Reorders a selected face by putting it before the specified face.
Indices start at 0 for the 1st element.
Signature
ReorderBeforeFaceNode(parentTag, faceSetIndexToMove, faceSetIndexToReoderBefore)
Parameters: - parentTag (
NXOpen.NXObject
) – Parent Weld Feature. - faceSetIndexToMove (int) – Index of the face set to reorder
- faceSetIndexToReoderBefore (int) – Index of the face set to reposition before
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
- parentTag (
RequiredFaceNode¶
-
ConnectionFinderBuilder.
RequiredFaceNode
¶ Identify if the face node is required (true) or optional (false).
This is used in the case where a weld point has been identified as having faces from only 1 connected part.
Signature
RequiredFaceNode(nodeTag, isRequired)
Parameters: - nodeTag (
NXOpen.NXObject
) – Weld face identifier. Typically, this will be the tag for the collector. - isRequired (bool) – Is the face node required (true) or optional (false)?
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
- nodeTag (
SaveAllTree¶
-
ConnectionFinderBuilder.
SaveAllTree
¶ Identify all the connected part information as “saved” so the commit will save the information.
Dependent on value of
NXOpen.Weld.ConnectionFinderBuilderFilterTypes
. Will not mark nodes identified in failure condition.Signature
SaveAllTree()
New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
SaveNode¶
-
ConnectionFinderBuilder.
SaveNode
¶ Identify the connected part information as “saved” so commit will save the information.
Signature
SaveNode(nodeTag)
Parameters: nodeTag ( NXOpen.NXObject
) – Weld Feature.New in version NX9.0.0.
License requirements: ugweld (“UG WELD”)
Validate¶
-
ConnectionFinderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.