CharacteristicsSelectionBuilder Class¶
-
class
NXOpen.Weld.
CharacteristicsSelectionBuilder
¶ Bases:
NXOpen.NXObject
This builder allows you to define the attribute values to be set on the output of the weld feature.
The inheritance option only applies to the
NXOpen.Weld.WeldJoint
.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AttributeList | Returns the list of potential attributes for this weld feature. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
SelectObjectList | Returns the selection object containing data that is to be attributed. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
CreateAttributeListEntry | Create an attribute list entry, that has no value, and add it to the list. |
CreateDoubleAttributeListEntry | Create a double attribute list entry and add it to the list. |
CreateIntegerAttributeListEntry | Create an integer attribute list entry and add it to the list. |
CreateOptionAttributeListEntry | Create an option attribute list entry and add it to the list. |
CreateStringAttributeListEntry | Create a string attribute list entry and add it to the list. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
AttributeList¶
-
CharacteristicsSelectionBuilder.
AttributeList
¶ Returns the list of potential attributes for this weld feature.
-------------------------------------
Getter Method
Signature
AttributeList
Returns: Return type: NXOpen.NXObjectList
New in version NX7.5.0.
License requirements: None.
IsOccurrence¶
-
CharacteristicsSelectionBuilder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CharacteristicsSelectionBuilder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CharacteristicsSelectionBuilder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CharacteristicsSelectionBuilder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CharacteristicsSelectionBuilder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CharacteristicsSelectionBuilder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SelectObjectList¶
-
CharacteristicsSelectionBuilder.
SelectObjectList
¶ Returns the selection object containing data that is to be attributed.
-------------------------------------
Getter Method
Signature
SelectObjectList
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreateAttributeListEntry¶
-
CharacteristicsSelectionBuilder.
CreateAttributeListEntry
¶ Overloaded method CreateAttributeListEntry
CreateAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title)
CreateAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title)
-------------------------------------
Create an attribute list entry, that has no value, and add it to the list.
Signature
CreateAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
Returns: Return type: New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Weld.CharacteristicsSelectionBuilder.CreateAttributeListEntry()
with inherited parameter instead.License requirements: None.
-------------------------------------
Create an attribute list entry, that has no value, and add it to the list.
Signature
CreateAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- inherited (bool) – Is attribute to be inherited, and over-written, by a source entity attribute? Only used by certain application tools.
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
Returns: Return type: New in version NX10.0.0.
License requirements: None.
-------------------------------------
CreateDoubleAttributeListEntry¶
-
CharacteristicsSelectionBuilder.
CreateDoubleAttributeListEntry
¶ Overloaded method CreateDoubleAttributeListEntry
CreateDoubleAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue)
CreateDoubleAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue)
-------------------------------------
Create a double attribute list entry and add it to the list.
Signature
CreateDoubleAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (float) – Current value setting of attribute.
Returns: Return type: New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Weld.CharacteristicsSelectionBuilder.CreateDoubleAttributeListEntry()
with inherited parameter instead.License requirements: None.
-------------------------------------
Create a double attribute list entry and add it to the list.
Signature
CreateDoubleAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- inherited (bool) – Is attribute to be inherited, and over-written, by a source entity attribute? Only used by certain application tools.
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (float) – Current value setting of attribute.
Returns: Return type: New in version NX10.0.0.
License requirements: None.
-------------------------------------
CreateIntegerAttributeListEntry¶
-
CharacteristicsSelectionBuilder.
CreateIntegerAttributeListEntry
¶ Overloaded method CreateIntegerAttributeListEntry
CreateIntegerAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue)
CreateIntegerAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue)
-------------------------------------
Create an integer attribute list entry and add it to the list.
Signature
CreateIntegerAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (int) – Current value setting of attribute.
Returns: Return type: New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Weld.CharacteristicsSelectionBuilder.CreateIntegerAttributeListEntry()
with inherited parameter instead.License requirements: None.
-------------------------------------
Create an integer attribute list entry and add it to the list.
Signature
CreateIntegerAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- inherited (bool) – Is attribute to be inherited, and over-written, by a source entity attribute? Only used by certain application tools.
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (int) – Current value setting of attribute.
Returns: Return type: New in version NX10.0.0.
License requirements: None.
-------------------------------------
CreateOptionAttributeListEntry¶
-
CharacteristicsSelectionBuilder.
CreateOptionAttributeListEntry
¶ Overloaded method CreateOptionAttributeListEntry
CreateOptionAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue, options)
CreateOptionAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue, options)
-------------------------------------
Create an option attribute list entry and add it to the list.
Signature
CreateOptionAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue, options)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (str) – Current value setting of attribute.
- options (list of str) – Options available to be chosen.
Returns: Return type: New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Weld.CharacteristicsSelectionBuilder.CreateOptionAttributeListEntry()
with inherited parameter instead.License requirements: None.
-------------------------------------
Create an option attribute list entry and add it to the list.
Signature
CreateOptionAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue, options)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- inherited (bool) – Is attribute to be inherited, and over-written, by a source entity attribute? Only used by certain application tools.
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (str) – Current value setting of attribute.
- options (list of str) – Options available to be chosen.
Returns: Return type: New in version NX10.0.0.
License requirements: None.
-------------------------------------
CreateStringAttributeListEntry¶
-
CharacteristicsSelectionBuilder.
CreateStringAttributeListEntry
¶ Overloaded method CreateStringAttributeListEntry
CreateStringAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue)
CreateStringAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue)
-------------------------------------
Create a string attribute list entry and add it to the list.
Signature
CreateStringAttributeListEntry(required, onObject, locked, iconName, pointMarker, color, title, currentValue)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (str) – Current value setting of attribute.
Returns: Return type: New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Weld.CharacteristicsSelectionBuilder.CreateStringAttributeListEntry()
with inherited parameter instead.License requirements: None.
-------------------------------------
Create a string attribute list entry and add it to the list.
Signature
CreateStringAttributeListEntry(required, onObject, locked, inherited, iconName, pointMarker, color, title, currentValue)
Parameters: - required (bool) – Is attribute required to be on output object?
- onObject (bool) – Is attribute already on existing object?
- locked (bool) – Is attribute locked?
- inherited (bool) – Is attribute to be inherited, and over-written, by a source entity attribute? Only used by certain application tools.
- iconName (str) – Name of icon to place in list.
- pointMarker (int) – marker to apply to point representing weld spot, see POINT_marker_t in point.h.
- color (int) – color to apply to object.
- title (str) – Title of attribute.
- currentValue (str) – Current value setting of attribute.
Returns: Return type: New in version NX10.0.0.
License requirements: None.
-------------------------------------
FindObject¶
-
CharacteristicsSelectionBuilder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
CharacteristicsSelectionBuilder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
CharacteristicsSelectionBuilder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.