CharacteristicsValueBuilder Class¶
-
class
NXOpen.Weld.
CharacteristicsValueBuilder
¶ Bases:
NXOpen.NXObject
The object containing the information about the attribute to be placed on the output of the weld feature.
The inheritance option only applies to the
NXOpen.Weld.WeldJoint
.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Active | Returns or sets the indication if the attribute is to be placed on the output. |
AttributeType | Returns the type of this attribute. |
Inherited | Returns or sets the indication if the attribute value is inherited from the source object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Required | Returns the indication if the attribute is required to be placed on the output. |
Tag | Returns the Tag for this object. |
Title | Returns the title of this attribute. |
ValueChanged | Returns or sets the indication if the attribute value has been changed. |
ValueDouble | Returns or sets the value of this attribute when AttributeType is Weld.CharacteristicsValueBuilderType.Double . |
ValueInteger | Returns or sets the value of this attribute when AttributeType is Weld.CharacteristicsValueBuilderType.Integer . |
ValueString | Returns or sets the value of this attribute when AttributeType is Weld.CharacteristicsValueBuilderType.String or Weld.CharacteristicsValueBuilderType.Option . |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetOptionStrings | The list of strings that are available to be set when AttributeType is Weld.CharacteristicsValueBuilderType.Option . |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
CharacteristicsValueBuilderType Enumeration | Settings to indicate the type of value contained in the attribute. |
Property Detail¶
Active¶
-
CharacteristicsValueBuilder.
Active
¶ Returns or sets the indication if the attribute is to be placed on the output.
true indicates the attribute will be placed on the output, false indicates the attribute will not be placed on the output. Note that if Required is true, then this property cannot be set.
-------------------------------------
Getter Method
Signature
Active
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Active
Parameters: active (bool) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
AttributeType¶
-
CharacteristicsValueBuilder.
AttributeType
¶ Returns the type of this attribute.
-------------------------------------
Getter Method
Signature
AttributeType
Returns: Return type: NXOpen.Weld.CharacteristicsValueBuilderType
New in version NX7.5.0.
License requirements: None.
Inherited¶
-
CharacteristicsValueBuilder.
Inherited
¶ Returns or sets the indication if the attribute value is inherited from the source object.
-------------------------------------
Getter Method
Signature
Inherited
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Inherited
Parameters: inherited (bool) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”) OR structure_weld (“STRUCTURE WELD”)
IsOccurrence¶
-
CharacteristicsValueBuilder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CharacteristicsValueBuilder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CharacteristicsValueBuilder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CharacteristicsValueBuilder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CharacteristicsValueBuilder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CharacteristicsValueBuilder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Required¶
-
CharacteristicsValueBuilder.
Required
¶ Returns the indication if the attribute is required to be placed on the output.
true indicates the attribute will always be placed on the output, false indicates the attribute does not have to be placed on the output.
-------------------------------------
Getter Method
Signature
Required
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
Title¶
-
CharacteristicsValueBuilder.
Title
¶ Returns the title of this attribute.
-------------------------------------
Getter Method
Signature
Title
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
ValueChanged¶
-
CharacteristicsValueBuilder.
ValueChanged
¶ Returns or sets the indication if the attribute value has been changed.
-------------------------------------
Getter Method
Signature
ValueChanged
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueChanged
Parameters: status (bool) – New in version NX8.0.1.
License requirements: ugweld (“UG WELD”)
ValueDouble¶
-
CharacteristicsValueBuilder.
ValueDouble
¶ Returns or sets the value of this attribute when AttributeType is
Weld.CharacteristicsValueBuilderType.Double
.-------------------------------------
Getter Method
Signature
ValueDouble
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueDouble
Parameters: valueDouble (float) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
ValueInteger¶
-
CharacteristicsValueBuilder.
ValueInteger
¶ Returns or sets the value of this attribute when AttributeType is
Weld.CharacteristicsValueBuilderType.Integer
.-------------------------------------
Getter Method
Signature
ValueInteger
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueInteger
Parameters: valueInteger (int) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
ValueString¶
-
CharacteristicsValueBuilder.
ValueString
¶ Returns or sets the value of this attribute when AttributeType is
Weld.CharacteristicsValueBuilderType.String
orWeld.CharacteristicsValueBuilderType.Option
.-------------------------------------
Getter Method
Signature
ValueString
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueString
Parameters: valueString (str) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Method Detail¶
FindObject¶
-
CharacteristicsValueBuilder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetOptionStrings¶
-
CharacteristicsValueBuilder.
GetOptionStrings
¶ The list of strings that are available to be set when AttributeType is
Weld.CharacteristicsValueBuilderType.Option
.Signature
GetOptionStrings()
Returns: Strings that are allowed for values. Return type: list of str New in version NX7.5.0.
License requirements: None.
Print¶
-
CharacteristicsValueBuilder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
CharacteristicsValueBuilder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.