StylerEvent Class¶
-
class
NXOpen.UIStyler.
StylerEvent
¶ Bases:
NXOpen.TransientObject
Represents a StylerEvent
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetReason | Gets the reason for the event |
GetStylerItem | Gets the dialog item |
Enumerations¶
StylerEventIndicator Enumeration | Describes indicator value |
StylerEventMiscellaneous Enumeration | Describes event index |
StylerEventReason Enumeration | Describes callback reason |
Method Detail¶
Dispose¶
-
StylerEvent.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET or Java, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
GetReason¶
-
StylerEvent.
GetReason
¶ Gets the reason for the event
Signature
GetReason()
Returns: Reason Return type: NXOpen.UIStyler.StylerEventReason
New in version NX5.0.0.
License requirements: None.
GetStylerItem¶
-
StylerEvent.
GetStylerItem
¶ Gets the dialog item
Signature
GetStylerItem()
Returns: Return type: NXOpen.UIStyler.StylerItem
New in version NX5.0.0.
License requirements: None.