StylerItem Class¶
-
class
NXOpen.UIStyler.
StylerItem
¶ Bases:
NXOpen.TransientObject
Represents a Styler Item
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
Enumerations¶
StylerItemItemType Enumeration | Describes kind of action to be taken from callbac. |
Method Detail¶
Dispose¶
-
StylerItem.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET or Java, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
GetItemType¶
-
StylerItem.
GetItemType
¶ Gets the dialog item type.
User can write programs to query this attribute and determine the type of a dialog item in order to determine what further actions should be taken.
Signature
GetItemType()
Returns: Return type: NXOpen.UIStyler.StylerItemItemType
New in version NX5.0.0.
License requirements: None.
InitializeAttachment¶
-
StylerItem.
InitializeAttachment
¶ Returns initialized dialog item attachment information
Signature
InitializeAttachment()
Returns: attachment object Return type: NXOpen.UIStyler.Attachment
New in version NX5.0.0.
License requirements: None.
IsEqualTo¶
-
StylerItem.
IsEqualTo
¶ Equates two styler items
Signature
IsEqualTo(itemToCompare)
Parameters: itemToCompare ( NXOpen.UIStyler.StylerItem
) – styler item to compareReturns: Return type: bool New in version NX5.0.0.
License requirements: None.
SetAttachment¶
-
StylerItem.
SetAttachment
¶ Specifies the updated dialog item attachment information
Signature
SetAttachment(attachment)
Parameters: attachment ( NXOpen.UIStyler.Attachment
) – attachment objectNew in version NX5.0.0.
License requirements: None.