StylerEventReason Enumeration¶
NXOpen.UIStyler.StylerEvent.Reason is an alias for NXOpen.UIStyler.StylerEventReason
-
class
NXOpen.UIStyler.
StylerEventReason
¶ Bases:
object
Describes callback reason
Enum Members
Enum Member Enum Member Description NoReason No reason ActivateReason Activate reason ValueChangedReason Value changed reason DragReason Drag reason DoubleClickReason Double click reason OkReason Ok reason ApplyReason Apply reason BackReason BAck reason CancelReason Cancel reason ConstructReason Construct reason DestructReason Destruct reason FileopReason File operation reason SwitchReason Switch reason FileOperationReason File operation reason ExitFileOperationReason Exit file operation reason -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-