EjectorPostProcessingBuilder Class¶
-
class
NXOpen.Tooling.
EjectorPostProcessingBuilder
¶ Bases:
NXOpen.Builder
Represents a builder to be used to create Mold Wizard ejector post processing.
To create a new instance of this class, use
NXOpen.Tooling.EjectorPostProcessingCollection.CreateEjectorPostProcessingBuilder()
Default values.
Property Value ActionType AdjustLength ForceFitDistance 0 PrecisionValue 0 TrimPart Notrimpart TrimSurface Face New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ActionType | Returns or sets the trim method of ejector pin post processing. |
FitDistance | Returns the distance used to adjust the length of an ejector pin for the false body |
ForceFitDistance | Returns or sets the option is used to determine whether or not to force the use of the fit distance value from the UI, instead of the value from the ejector pin part |
OffsetValue | Returns the offset value is used to create offset feature on the trimmed ejector pin true body. |
PrecisionValue | Returns or sets the precision of the fit distance value. |
Tag | Returns the Tag for this object. |
TargetComponents | Returns the target components which contains the target ejector pins to be trimmed. |
ToolFace | Returns the faces used to trim an ejector pin. |
ToolSheetBody | Returns the sheet body used to trim an ejector pin. |
TrimPart | Returns or sets the trim part in which trim surface features are cycled. |
TrimSurface | Returns or sets the trim surface used to trim an ejector pin. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetTrimDataDetails | Set details of the trim data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EjectorPostProcessingBuilderTrimMethod Enumeration | The processing type: Trim, Adjust length and Untrim. |
EjectorPostProcessingBuilderTrimPartName Enumeration | The trim part where to find a trim surface as tool to trim ejector pins. |
EjectorPostProcessingBuilderTrimSufaceName Enumeration | The trim surface types. |
Property Detail¶
ActionType¶
-
EjectorPostProcessingBuilder.
ActionType
¶ Returns or sets the trim method of ejector pin post processing.
-------------------------------------
Getter Method
Signature
ActionType
Returns: Return type: NXOpen.Tooling.EjectorPostProcessingBuilderTrimMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActionType
Parameters: actionType ( NXOpen.Tooling.EjectorPostProcessingBuilderTrimMethod
) –New in version NX7.5.0.
License requirements: None.
FitDistance¶
-
EjectorPostProcessingBuilder.
FitDistance
¶ Returns the distance used to adjust the length of an ejector pin for the false body
-------------------------------------
Getter Method
Signature
FitDistance
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ForceFitDistance¶
-
EjectorPostProcessingBuilder.
ForceFitDistance
¶ Returns or sets the option is used to determine whether or not to force the use of the fit distance value from the UI, instead of the value from the ejector pin part
-------------------------------------
Getter Method
Signature
ForceFitDistance
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForceFitDistance
Parameters: forceFitDistance (bool) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”)
OffsetValue¶
-
EjectorPostProcessingBuilder.
OffsetValue
¶ Returns the offset value is used to create offset feature on the trimmed ejector pin true body.
-------------------------------------
Getter Method
Signature
OffsetValue
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
PrecisionValue¶
-
EjectorPostProcessingBuilder.
PrecisionValue
¶ Returns or sets the precision of the fit distance value.
-------------------------------------
Getter Method
Signature
PrecisionValue
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrecisionValue
Parameters: precisionValue (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”)
TargetComponents¶
-
EjectorPostProcessingBuilder.
TargetComponents
¶ Returns the target components which contains the target ejector pins to be trimmed.
-------------------------------------
Getter Method
Signature
TargetComponents
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: None.
ToolFace¶
-
EjectorPostProcessingBuilder.
ToolFace
¶ Returns the faces used to trim an ejector pin.
-------------------------------------
Getter Method
Signature
ToolFace
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
ToolSheetBody¶
-
EjectorPostProcessingBuilder.
ToolSheetBody
¶ Returns the sheet body used to trim an ejector pin.
-------------------------------------
Getter Method
Signature
ToolSheetBody
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
TrimPart¶
-
EjectorPostProcessingBuilder.
TrimPart
¶ Returns or sets the trim part in which trim surface features are cycled.
-------------------------------------
Getter Method
Signature
TrimPart
Returns: Return type: NXOpen.Tooling.EjectorPostProcessingBuilderTrimPartName
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimPart
Parameters: trimPart ( NXOpen.Tooling.EjectorPostProcessingBuilderTrimPartName
) –New in version NX7.5.0.
License requirements: None.
TrimSurface¶
-
EjectorPostProcessingBuilder.
TrimSurface
¶ Returns or sets the trim surface used to trim an ejector pin.
-------------------------------------
Getter Method
Signature
TrimSurface
Returns: Return type: NXOpen.Tooling.EjectorPostProcessingBuilderTrimSufaceName
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimSurface
Parameters: trimSurface ( NXOpen.Tooling.EjectorPostProcessingBuilderTrimSufaceName
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
SetTrimDataDetails¶
-
EjectorPostProcessingBuilder.
SetTrimDataDetails
¶ Set details of the trim data.
Signature
SetTrimDataDetails(surfaceType, targets, tools)
Parameters: - surfaceType (int) – the surface type.
- targets (list of
NXOpen.NXObject
) – array of target ejector pins. - tools (list of
NXOpen.NXObject
) – array of tool objects.
New in version NX7.5.0.
License requirements: None.
Validate¶
-
EjectorPostProcessingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.