DieEngFormTaskBuilder Class¶
-
class
NXOpen.Tooling.
DieEngFormTaskBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Form Task builder
To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateDieEngFormTaskBuilder()
Default values.
Property Value FinishOperation 1 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CamDirection | Returns or sets the cam direction. |
DieTip | Returns the die tip selection. |
FinishOperation | Returns or sets the finish operation option. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PointInRegion | Returns or sets the point in region |
RegionBounds | Returns the edge region bounds |
ShapeDetail | Returns the shape detail selection. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDetails | Returns the detailed information of the feature set by user. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetDetails | Sets the detailed information of the feature. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CamDirection¶
-
DieEngFormTaskBuilder.
CamDirection
¶ Returns or sets the cam direction.
-------------------------------------
Getter Method
Signature
CamDirection
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CamDirection
Parameters: camDirection ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DieTip¶
-
DieEngFormTaskBuilder.
DieTip
¶ Returns the die tip selection.
-------------------------------------
Getter Method
Signature
DieTip
Returns: Return type: NXOpen.Features.SelectFeature
New in version NX8.0.0.
License requirements: None.
FinishOperation¶
-
DieEngFormTaskBuilder.
FinishOperation
¶ Returns or sets the finish operation option.
-------------------------------------
Getter Method
Signature
FinishOperation
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FinishOperation
Parameters: finishOperation (bool) – New in version NX8.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PointInRegion¶
-
DieEngFormTaskBuilder.
PointInRegion
¶ Returns or sets the point in region
-------------------------------------
Getter Method
Signature
PointInRegion
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointInRegion
Parameters: pointInRegion ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
RegionBounds¶
-
DieEngFormTaskBuilder.
RegionBounds
¶ Returns the edge region bounds
-------------------------------------
Getter Method
Signature
RegionBounds
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
ShapeDetail¶
-
DieEngFormTaskBuilder.
ShapeDetail
¶ Returns the shape detail selection.
-------------------------------------
Getter Method
Signature
ShapeDetail
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetDetails¶
-
DieEngFormTaskBuilder.
GetDetails
¶ Returns the detailed information of the feature set by user.
Signature
GetDetails()
Returns: Return type: list of str New in version NX8.0.0.
License requirements: None.
SetDetails¶
-
DieEngFormTaskBuilder.
SetDetails
¶ Sets the detailed information of the feature.
Signature
SetDetails(details)
Parameters: details (list of str) – New in version NX8.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Validate¶
-
DieEngFormTaskBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.