DieCavityAndSlugHoleBuilder Class¶
-
class
NXOpen.Tooling.
DieCavityAndSlugHoleBuilder
¶ Bases:
NXOpen.Builder
Represents die cavity and slug hole builder.
To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateDieCavityAndSlugHoleBuilder()
Default values.
Property Value AngleDiePlateTwo -0.25 DieInsertStack One DieOffsetValue 0 DiePlateThree 2 DiePlateTwo 1 DieSameOffsetValue 0 ForEachScrapDiePlateThree 1 ForEachScrapDiePlateTwo 1 NormalBottomBackPlateSlug Fillet NormalCavity TaperAngle NormalClearance 0.05 NormalClearanceOption Constant NormalDieShoeSlug Fillet NormalForEachScrap1 0 NormalForEachScrap2 0 NormalOffsetSide DieSide NormalRenameDialog 0 NormalSlugInDiePlateThree Fillet NormalSlugInDiePlateTwo Fillet NormalSlugParameter1 3 NormalSlugParameter2 -3 NormalSlugParameter3 2 NormalSlugParameter4 3 OffsetLinearDimension.Value 3 (millimeters part), 0.12 (inches part) Position Bottom ShimHeight 0 ShimOffset 0 SlugHoleHeightLinearDimension.Value 100 (millimeters part), 4 (inches part) SpacerAngle 0 SpacerOffset 0 WaferHeight 0 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AngleDiePlateTwo | Returns or sets the angle of the die plate two |
DieInsertStack | Returns or sets the die insert stack |
DieOffsetValue | Returns or sets the die offset value |
DiePlateThree | Returns or sets the die plate three |
DiePlateTwo | Returns or sets the die plate two |
DieSameOffsetValue | Returns or sets the die same offset value |
ForEachScrapDiePlateThree | Returns or sets the result whether use same clearance for each scrap in die plate three |
ForEachScrapDiePlateTwo | Returns or sets the for each scrap die plate two |
NewPartNames | Returns or sets the new component names. |
NormalBottomBackPlateSlug | Returns or sets the normal bbpslug |
NormalCavity | Returns or sets the normal cavity |
NormalClearance | Returns or sets the normal clearance |
NormalClearanceOption | Returns or sets the normal clearance option |
NormalDieShoeSlug | Returns or sets the normal dsslug |
NormalForEachScrap1 | Returns or sets the normal for each scrap1 |
NormalForEachScrap2 | Returns or sets the normal for each scrap2 |
NormalOffsetSide | Returns or sets the normal offset side |
NormalRenameDialog | Returns or sets the normal rename dialog |
NormalSelectPierceDieInsert | Returns the normal select pierce die insert |
NormalSlugInDiePlateThree | Returns or sets the normal slug in diePlateThree |
NormalSlugInDiePlateTwo | Returns or sets the normal slug in die plate two |
NormalSlugParameter1 | Returns or sets the normal slug parameter1 |
NormalSlugParameter2 | Returns or sets the normal slug parameter2 |
NormalSlugParameter3 | Returns or sets the normal slug parameter3 |
NormalSlugParameter4 | Returns or sets the normal slug parameter4 |
OffsetLinearDimension | Returns the offset linear dimension |
ParentPartName | Returns or sets the parent part name to create insert. |
Position | Returns or sets the position |
SelectOffsetSpreadsheet | Returns or sets the super offset spreadsheet |
SelectScrap | Returns the select scrap |
SelectSketch | Returns the select sketch |
ShimHeight | Returns or sets the shim height |
ShimOffset | Returns or sets the shim offset |
SlugHoleHeightLinearDimension | Returns the slug hole height linear dimension |
SlugPreviousParameterA | Returns or sets the previous slug parameter A |
SlugPreviousParameterC1 | Returns or sets the previous slug parameter C1 |
SlugPreviousParameterC2 | Returns or sets the previous slug parameter C2 |
SpacerAngle | Returns or sets the spacer angle |
SpacerOffset | Returns or sets the spacer offset |
Tag | Returns the Tag for this object. |
WaferHeight | Returns or sets the wafer height |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DieEditOffsetValueTable | Edit offset value table for die |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
NormalCreateCavityAndSlug | Create normal cavity and slug |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DieCavityAndSlugHoleBuilderBottomPlateSlugItems Enumeration | Specifies the type of bottom plate slug. |
DieCavityAndSlugHoleBuilderCavityTypeItems Enumeration | Specifies the type of cavity. |
DieCavityAndSlugHoleBuilderClearanceOptionItems Enumeration | Specifies the design option of piercing insert. |
DieCavityAndSlugHoleBuilderDieInsertStackType Enumeration | die insert stack type. |
DieCavityAndSlugHoleBuilderDiePlateThreeSlugType Enumeration | die plate three slug type. |
DieCavityAndSlugHoleBuilderDiePlateTwoSlugType Enumeration | die plate two slug type. |
DieCavityAndSlugHoleBuilderDieShoeSlugTypeItems Enumeration | Specifies the type of die shoe slug. |
DieCavityAndSlugHoleBuilderInsertPositionItems Enumeration | Specifies the position of piercing inserts, for EDW only |
DieCavityAndSlugHoleBuilderOffsetSideOptionItems Enumeration | Specifies the offset side of normal pierce insert design. |
Property Detail¶
AngleDiePlateTwo¶
-
DieCavityAndSlugHoleBuilder.
AngleDiePlateTwo
¶ Returns or sets the angle of the die plate two
-------------------------------------
Getter Method
Signature
AngleDiePlateTwo
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleDiePlateTwo
Parameters: angleDiePlateTwo (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
DieInsertStack¶
-
DieCavityAndSlugHoleBuilder.
DieInsertStack
¶ Returns or sets the die insert stack
-------------------------------------
Getter Method
Signature
DieInsertStack
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderDieInsertStackType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DieInsertStack
Parameters: dieInsertStack ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderDieInsertStackType
) –New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
DieOffsetValue¶
-
DieCavityAndSlugHoleBuilder.
DieOffsetValue
¶ Returns or sets the die offset value
-------------------------------------
Getter Method
Signature
DieOffsetValue
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DieOffsetValue
Parameters: dieOffsetValue (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DiePlateThree¶
-
DieCavityAndSlugHoleBuilder.
DiePlateThree
¶ Returns or sets the die plate three
-------------------------------------
Getter Method
Signature
DiePlateThree
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiePlateThree
Parameters: diePlateThree (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
DiePlateTwo¶
-
DieCavityAndSlugHoleBuilder.
DiePlateTwo
¶ Returns or sets the die plate two
-------------------------------------
Getter Method
Signature
DiePlateTwo
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiePlateTwo
Parameters: diePlateTwo (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
DieSameOffsetValue¶
-
DieCavityAndSlugHoleBuilder.
DieSameOffsetValue
¶ Returns or sets the die same offset value
-------------------------------------
Getter Method
Signature
DieSameOffsetValue
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DieSameOffsetValue
Parameters: dieSameOffsetValue (bool) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ForEachScrapDiePlateThree¶
-
DieCavityAndSlugHoleBuilder.
ForEachScrapDiePlateThree
¶ Returns or sets the result whether use same clearance for each scrap in die plate three
-------------------------------------
Getter Method
Signature
ForEachScrapDiePlateThree
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForEachScrapDiePlateThree
Parameters: forEachScrapDiePlateThree (bool) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ForEachScrapDiePlateTwo¶
-
DieCavityAndSlugHoleBuilder.
ForEachScrapDiePlateTwo
¶ Returns or sets the for each scrap die plate two
-------------------------------------
Getter Method
Signature
ForEachScrapDiePlateTwo
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForEachScrapDiePlateTwo
Parameters: forEachScrapDiePlateTwo (bool) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
NewPartNames¶
-
DieCavityAndSlugHoleBuilder.
NewPartNames
¶ Returns or sets the new component names.
-------------------------------------
Getter Method
Signature
NewPartNames
Returns: Retruns the new component names Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewPartNames
Parameters: newPartNames (str) – Specifies the new component names New in version NX11.0.0.
License requirements: None.
NormalBottomBackPlateSlug¶
-
DieCavityAndSlugHoleBuilder.
NormalBottomBackPlateSlug
¶ Returns or sets the normal bbpslug
-------------------------------------
Getter Method
Signature
NormalBottomBackPlateSlug
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderBottomPlateSlugItems
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalBottomBackPlateSlug
Parameters: normalBottomBackPlateSlug ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderBottomPlateSlugItems
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalCavity¶
-
DieCavityAndSlugHoleBuilder.
NormalCavity
¶ Returns or sets the normal cavity
-------------------------------------
Getter Method
Signature
NormalCavity
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderCavityTypeItems
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalCavity
Parameters: normalCavity ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderCavityTypeItems
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalClearance¶
-
DieCavityAndSlugHoleBuilder.
NormalClearance
¶ Returns or sets the normal clearance
-------------------------------------
Getter Method
Signature
NormalClearance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalClearance
Parameters: normalClearance (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalClearanceOption¶
-
DieCavityAndSlugHoleBuilder.
NormalClearanceOption
¶ Returns or sets the normal clearance option
-------------------------------------
Getter Method
Signature
NormalClearanceOption
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderClearanceOptionItems
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalClearanceOption
Parameters: normalClearanceOption ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderClearanceOptionItems
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalDieShoeSlug¶
-
DieCavityAndSlugHoleBuilder.
NormalDieShoeSlug
¶ Returns or sets the normal dsslug
-------------------------------------
Getter Method
Signature
NormalDieShoeSlug
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderDieShoeSlugTypeItems
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalDieShoeSlug
Parameters: normalDieShoeSlug ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderDieShoeSlugTypeItems
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalForEachScrap1¶
-
DieCavityAndSlugHoleBuilder.
NormalForEachScrap1
¶ Returns or sets the normal for each scrap1
-------------------------------------
Getter Method
Signature
NormalForEachScrap1
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalForEachScrap1
Parameters: normalForEachScrap1 (bool) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalForEachScrap2¶
-
DieCavityAndSlugHoleBuilder.
NormalForEachScrap2
¶ Returns or sets the normal for each scrap2
-------------------------------------
Getter Method
Signature
NormalForEachScrap2
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalForEachScrap2
Parameters: normalForEachScrap2 (bool) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalOffsetSide¶
-
DieCavityAndSlugHoleBuilder.
NormalOffsetSide
¶ Returns or sets the normal offset side
-------------------------------------
Getter Method
Signature
NormalOffsetSide
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderOffsetSideOptionItems
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalOffsetSide
Parameters: normalOffsetSide ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderOffsetSideOptionItems
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalRenameDialog¶
-
DieCavityAndSlugHoleBuilder.
NormalRenameDialog
¶ Returns or sets the normal rename dialog
-------------------------------------
Getter Method
Signature
NormalRenameDialog
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalRenameDialog
Parameters: normalRenameDialog (bool) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalSelectPierceDieInsert¶
-
DieCavityAndSlugHoleBuilder.
NormalSelectPierceDieInsert
¶ Returns the normal select pierce die insert
-------------------------------------
Getter Method
Signature
NormalSelectPierceDieInsert
Returns: Return type: NXOpen.SelectBodyList
New in version NX11.0.0.
License requirements: None.
NormalSlugInDiePlateThree¶
-
DieCavityAndSlugHoleBuilder.
NormalSlugInDiePlateThree
¶ Returns or sets the normal slug in diePlateThree
-------------------------------------
Getter Method
Signature
NormalSlugInDiePlateThree
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderDiePlateThreeSlugType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalSlugInDiePlateThree
Parameters: normalSlugInDiePlateThree ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderDiePlateThreeSlugType
) –New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
NormalSlugInDiePlateTwo¶
-
DieCavityAndSlugHoleBuilder.
NormalSlugInDiePlateTwo
¶ Returns or sets the normal slug in die plate two
-------------------------------------
Getter Method
Signature
NormalSlugInDiePlateTwo
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderDiePlateTwoSlugType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalSlugInDiePlateTwo
Parameters: normalSlugInDiePlateTwo ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderDiePlateTwoSlugType
) –New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
NormalSlugParameter1¶
-
DieCavityAndSlugHoleBuilder.
NormalSlugParameter1
¶ Returns or sets the normal slug parameter1
-------------------------------------
Getter Method
Signature
NormalSlugParameter1
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalSlugParameter1
Parameters: normalSlugParameter1 (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalSlugParameter2¶
-
DieCavityAndSlugHoleBuilder.
NormalSlugParameter2
¶ Returns or sets the normal slug parameter2
-------------------------------------
Getter Method
Signature
NormalSlugParameter2
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalSlugParameter2
Parameters: normalSlugParameter2 (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalSlugParameter3¶
-
DieCavityAndSlugHoleBuilder.
NormalSlugParameter3
¶ Returns or sets the normal slug parameter3
-------------------------------------
Getter Method
Signature
NormalSlugParameter3
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalSlugParameter3
Parameters: normalSlugParameter3 (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalSlugParameter4¶
-
DieCavityAndSlugHoleBuilder.
NormalSlugParameter4
¶ Returns or sets the normal slug parameter4
-------------------------------------
Getter Method
Signature
NormalSlugParameter4
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalSlugParameter4
Parameters: normalSlugParameter4 (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetLinearDimension¶
-
DieCavityAndSlugHoleBuilder.
OffsetLinearDimension
¶ Returns the offset linear dimension
-------------------------------------
Getter Method
Signature
OffsetLinearDimension
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
ParentPartName¶
-
DieCavityAndSlugHoleBuilder.
ParentPartName
¶ Returns or sets the parent part name to create insert.
-------------------------------------
Getter Method
Signature
ParentPartName
Returns: Retruns parent part name Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPartName
Parameters: parentPartName (str) – Specifies the parent part name New in version NX11.0.0.
License requirements: None.
Position¶
-
DieCavityAndSlugHoleBuilder.
Position
¶ Returns or sets the position
-------------------------------------
Getter Method
Signature
Position
Returns: Return type: NXOpen.Tooling.DieCavityAndSlugHoleBuilderInsertPositionItems
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Position
Parameters: position ( NXOpen.Tooling.DieCavityAndSlugHoleBuilderInsertPositionItems
) –New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectOffsetSpreadsheet¶
-
DieCavityAndSlugHoleBuilder.
SelectOffsetSpreadsheet
¶ Returns or sets the super offset spreadsheet
-------------------------------------
Getter Method
Signature
SelectOffsetSpreadsheet
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectOffsetSpreadsheet
Parameters: filename (str) – New in version NX11.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SelectScrap¶
-
DieCavityAndSlugHoleBuilder.
SelectScrap
¶ Returns the select scrap
-------------------------------------
Getter Method
Signature
SelectScrap
Returns: Return type: NXOpen.SelectBodyList
New in version NX11.0.0.
License requirements: None.
SelectSketch¶
-
DieCavityAndSlugHoleBuilder.
SelectSketch
¶ Returns the select sketch
-------------------------------------
Getter Method
Signature
SelectSketch
Returns: Return type: NXOpen.SelectSketch
New in version NX11.0.0.
License requirements: None.
ShimHeight¶
-
DieCavityAndSlugHoleBuilder.
ShimHeight
¶ Returns or sets the shim height
-------------------------------------
Getter Method
Signature
ShimHeight
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShimHeight
Parameters: shimHeight (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ShimOffset¶
-
DieCavityAndSlugHoleBuilder.
ShimOffset
¶ Returns or sets the shim offset
-------------------------------------
Getter Method
Signature
ShimOffset
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShimOffset
Parameters: shimOffset (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SlugHoleHeightLinearDimension¶
-
DieCavityAndSlugHoleBuilder.
SlugHoleHeightLinearDimension
¶ Returns the slug hole height linear dimension
-------------------------------------
Getter Method
Signature
SlugHoleHeightLinearDimension
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
SlugPreviousParameterA¶
-
DieCavityAndSlugHoleBuilder.
SlugPreviousParameterA
¶ Returns or sets the previous slug parameter A
-------------------------------------
Getter Method
Signature
SlugPreviousParameterA
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SlugPreviousParameterA
Parameters: slugPreviousParameterA (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SlugPreviousParameterC1¶
-
DieCavityAndSlugHoleBuilder.
SlugPreviousParameterC1
¶ Returns or sets the previous slug parameter C1
-------------------------------------
Getter Method
Signature
SlugPreviousParameterC1
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SlugPreviousParameterC1
Parameters: slugPreviousParameterC1 (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SlugPreviousParameterC2¶
-
DieCavityAndSlugHoleBuilder.
SlugPreviousParameterC2
¶ Returns or sets the previous slug parameter C2
-------------------------------------
Getter Method
Signature
SlugPreviousParameterC2
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SlugPreviousParameterC2
Parameters: slugPreviousParameterC2 (float) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SpacerAngle¶
-
DieCavityAndSlugHoleBuilder.
SpacerAngle
¶ Returns or sets the spacer angle
-------------------------------------
Getter Method
Signature
SpacerAngle
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpacerAngle
Parameters: spacerAngle (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SpacerOffset¶
-
DieCavityAndSlugHoleBuilder.
SpacerOffset
¶ Returns or sets the spacer offset
-------------------------------------
Getter Method
Signature
SpacerOffset
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpacerOffset
Parameters: spacerOffset (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
WaferHeight¶
-
DieCavityAndSlugHoleBuilder.
WaferHeight
¶ Returns or sets the wafer height
-------------------------------------
Getter Method
Signature
WaferHeight
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WaferHeight
Parameters: waferHeight (float) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
DieEditOffsetValueTable¶
-
DieCavityAndSlugHoleBuilder.
DieEditOffsetValueTable
¶ Edit offset value table for die
Signature
DieEditOffsetValueTable()
New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
NormalCreateCavityAndSlug¶
-
DieCavityAndSlugHoleBuilder.
NormalCreateCavityAndSlug
¶ Create normal cavity and slug
Signature
NormalCreateCavityAndSlug()
New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
DieCavityAndSlugHoleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.