DieCavityAndSlugHoleBuilderCavityTypeItems Enumeration¶
NXOpen.Tooling.DieCavityAndSlugHoleBuilder.CavityTypeItems is an alias for NXOpen.Tooling.DieCavityAndSlugHoleBuilderCavityTypeItems
-
class
NXOpen.Tooling.
DieCavityAndSlugHoleBuilderCavityTypeItems
¶ Bases:
object
Specifies the type of cavity.
Enum Members
Enum Member Enum Member Description TaperAngle the taper angle type Step the step type RoundStep1 the round step1 type RoundStep2 the round step2 type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-