DieCavityAndSlugHoleBuilderInsertPositionItems Enumeration¶
NXOpen.Tooling.DieCavityAndSlugHoleBuilder.InsertPositionItems is an alias for NXOpen.Tooling.DieCavityAndSlugHoleBuilderInsertPositionItems
-
class
NXOpen.Tooling.
DieCavityAndSlugHoleBuilderInsertPositionItems
¶ Bases:
object
Specifies the position of piercing inserts, for EDW only
Enum Members
Enum Member Enum Member Description Top The position is top side Bottom The position is bottom side -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-