AddReusableFeatureCollectionInputData_Struct Struct¶
NXOpen.Tooling.AddReusableFeatureCollection.InputData is an alias for NXOpen.Tooling.AddReusableFeatureCollectionInputData_Struct
-
class
NXOpen.Tooling.
AddReusableFeatureCollectionInputData_Struct
¶ Bases:
object
Defines the input data of AddReusableFeatureBuilder .
Constructor: NXOpen.Tooling.AddReusableFeatureCollection.InputData()
Fields¶
Field | Description |
---|---|
KrxFile | KRX file of reusable feature template |
LibName | Library name of reusable feature template |
LibPath | Library path of reusable feature template |
Entity | Placement entity in create mode |
Position | Cursor position in create mode |
Feature | Reusable feature in edit mode |
KrxFile¶
-
AddReusableFeatureCollectionInputData_Struct.
KrxFile
¶ KRX file of reusable feature template
-------------------------------------
Field Value Type:str
LibName¶
-
AddReusableFeatureCollectionInputData_Struct.
LibName
¶ Library name of reusable feature template
-------------------------------------
Field Value Type:str
LibPath¶
-
AddReusableFeatureCollectionInputData_Struct.
LibPath
¶ Library path of reusable feature template
-------------------------------------
Field Value Type:str
Entity¶
-
AddReusableFeatureCollectionInputData_Struct.
Entity
¶ Placement entity in create mode
-------------------------------------
Field Value Type:
NXOpen.NXObject
Position¶
-
AddReusableFeatureCollectionInputData_Struct.
Position
¶ Cursor position in create mode
-------------------------------------
Field Value Type:
NXOpen.Point3d
Feature¶
-
AddReusableFeatureCollectionInputData_Struct.
Feature
¶ Reusable feature in edit mode
-------------------------------------
Field Value Type:
NXOpen.Features.Feature