SectionData Class¶
-
class
NXOpen.
SectionData
¶ Bases:
NXOpen.TransientObject
Represents section data
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetEndConnector | Gets end connector if any. |
GetRules | Return the selection intent rules |
GetSectionElementsData | Gets the section elements. |
GetStartConnector | Gets start connector if any. |
Method Detail¶
Dispose¶
-
SectionData.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetEndConnector¶
-
SectionData.
GetEndConnector
¶ Gets end connector if any.
It can be point, curve or edge
Signature
GetEndConnector()
Returns: Return type: NXOpen.NXObject
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
GetRules¶
-
SectionData.
GetRules
¶ Return the selection intent rules
See documentation for
NXOpen.SelectionIntentRule
for more details.Signature
GetRules()
Returns: Selection intent rules. Return type: list of NXOpen.SelectionIntentRule
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
GetSectionElementsData¶
-
SectionData.
GetSectionElementsData
¶ Gets the section elements.
See documentation for
NXOpen.SectionElementData
for more details.Signature
GetSectionElementsData()
Returns: Section elements Return type: list of NXOpen.SectionElementData
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
GetStartConnector¶
-
SectionData.
GetStartConnector
¶ Gets start connector if any.
It can be point, curve or edge
Signature
GetStartConnector()
Returns: Return type: NXOpen.NXObject
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)