SectionElementData Class¶
-
class
NXOpen.
SectionElementData
¶ Bases:
NXOpen.TransientObject
Represents section element data
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetSectionElementData | Gets the element that constructs the section |
GetSectionElementData1 | Gets the element that constructs the section |
Method Detail¶
Dispose¶
-
SectionElementData.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetSectionElementData¶
-
SectionElementData.
GetSectionElementData
¶ Gets the element that constructs the section
Signature
GetSectionElementData()
Returns: a tuple Return type: A tuple consisting of (sectionElement, startConnector, startPoint, endConnector, endPoint). sectionElement is a NXOpen.ICurve
. The element that constructs the section startConnector is aNXOpen.ICurve
. The element that is connected to the section_element, at the start_point startPoint is aNXOpen.Point3d
. Start pointendConnector is aNXOpen.ICurve
. The element that is connected to the section_element, at the end_pointendPoint is aNXOpen.Point3d
. End PointNew in version NX3.0.0.
Deprecated since version NX8.0.0: Use
SectionElementData.GetSectionElementData1()
instead.License requirements: gateway (“UG GATEWAY”)
GetSectionElementData1¶
-
SectionElementData.
GetSectionElementData1
¶ Gets the element that constructs the section
Signature
GetSectionElementData1()
Returns: a tuple Return type: A tuple consisting of (sectionElement, startConnector, startPoint, endConnector, endPoint). sectionElement is a NXOpen.DisplayableObject
. The element that constructs the section - this can be curve or point. startConnector is aNXOpen.DisplayableObject
. The element that is connected to the section_element, at the start_point - this can be curve or point startPoint is aNXOpen.Point3d
. Start pointendConnector is aNXOpen.DisplayableObject
. The element that is connected to the section_element, at the end_point - this can be curve or pointendPoint is aNXOpen.Point3d
. End PointNew in version NX8.0.0.
License requirements: gateway (“UG GATEWAY”)