SubdivideSegmentBuilder Class¶
-
class
NXOpen.Routing.
SubdivideSegmentBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.SubdivideSegmentBuilder
.This is used to subidivide a given segment into two or more segments based on one of the three spacing methods.
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateSubdivideSegmentBuilder()
Default values.
Property Value EqualSegmentsOption EqualArcLength SubdivideNumSegments 2 New in version NX6.0.0.
Properties¶
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSplineSettings | Gets the current subdivide spline settings. |
SetSplineSettings | Sets options for subdividing splines. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SubdivideSegmentBuilderEqualSegmentsMethod Enumeration | Options for subdivision with Equal Segments spacing method. |
SubdivideSegmentBuilderTypes Enumeration | Spacing method to use for subdivision. |
Property Detail¶
EqualSegmentsOption¶
-
SubdivideSegmentBuilder.
EqualSegmentsOption
¶ Returns or sets the equal segments option as
NXOpen.Routing.SubdivideSegmentBuilderEqualSegmentsMethod
-------------------------------------
Getter Method
Signature
EqualSegmentsOption
Returns: Return type: NXOpen.Routing.SubdivideSegmentBuilderEqualSegmentsMethod
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
EqualSegmentsOption
Parameters: equalSegmentsOption ( NXOpen.Routing.SubdivideSegmentBuilderEqualSegmentsMethod
) –New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
ReverseSubdividePoint¶
-
SubdivideSegmentBuilder.
ReverseSubdividePoint
¶ Returns or sets the direction of the start of segment to subdivide.
The distance of the subdivision point on the segment is measured from this end.
-------------------------------------
Getter Method
Signature
ReverseSubdividePoint
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ReverseSubdividePoint
Parameters: reverseSubdividePoint (bool) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Segment¶
-
SubdivideSegmentBuilder.
Segment
¶ Returns the segment to subdivide
-------------------------------------
Getter Method
Signature
Segment
Returns: Return type: NXOpen.Routing.SelectISegment
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SubdivideArcLength¶
-
SubdivideSegmentBuilder.
SubdivideArcLength
¶ Returns the arc length of each resulting segment from subdivision, if
NXOpen.Routing.SubdivideSegmentBuilderTypes
isNXOpen.Routing.SubdivideSegmentBuilderTypes.ArcLengthSegments
-------------------------------------
Getter Method
Signature
SubdivideArcLength
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SubdivideEndPercentage¶
-
SubdivideSegmentBuilder.
SubdivideEndPercentage
¶ Returns the end location of subdivision on the segment as percentage, if
NXOpen.Routing.SubdivideSegmentBuilderTypes
isNXOpen.Routing.SubdivideSegmentBuilderTypes.EqualSegments
orNXOpen.Routing.SubdivideSegmentBuilderTypes.ArcLengthSegments
-------------------------------------
Getter Method
Signature
SubdivideEndPercentage
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SubdivideNumSegments¶
-
SubdivideSegmentBuilder.
SubdivideNumSegments
¶ Returns or sets the number of subdivisions to do on the given segment, if
NXOpen.Routing.SubdivideSegmentBuilderTypes
isNXOpen.Routing.SubdivideSegmentBuilderTypes.EqualSegments
orNXOpen.Routing.SubdivideSegmentBuilderTypes.ArcLengthSegments
-------------------------------------
Getter Method
Signature
SubdivideNumSegments
Returns: Return type: int New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
SubdivideNumSegments
Parameters: subdivideNumSegments (int) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SubdividePoint¶
-
SubdivideSegmentBuilder.
SubdividePoint
¶ Returns the location of the subdivision point on segment as arclength or %arclength or point, if
NXOpen.Routing.SubdivideSegmentBuilderTypes
isNXOpen.Routing.SubdivideSegmentBuilderTypes.AtPoint
-------------------------------------
Getter Method
Signature
SubdividePoint
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SubdivideStartPercentage¶
-
SubdivideSegmentBuilder.
SubdivideStartPercentage
¶ Returns the start location of subdivision on the segment as percentage, if
NXOpen.Routing.SubdivideSegmentBuilderTypes
isNXOpen.Routing.SubdivideSegmentBuilderTypes.EqualSegments
orNXOpen.Routing.SubdivideSegmentBuilderTypes.ArcLengthSegments
-------------------------------------
Getter Method
Signature
SubdivideStartPercentage
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Type¶
-
SubdivideSegmentBuilder.
Type
¶ Returns or sets the spacing method as
NXOpen.Routing.SubdivideSegmentBuilderTypes
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Routing.SubdivideSegmentBuilderTypes
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Routing.SubdivideSegmentBuilderTypes
) –New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
GetSplineSettings¶
-
SubdivideSegmentBuilder.
GetSplineSettings
¶ Gets the current subdivide spline settings.
Signature
GetSplineSettings()
Returns: a tuple Return type: A tuple consisting of (createTangency, createPoints) createTangency is a bool. Creates tangency at the point where the spline is subdivided by adding parallel extensions.createPoints is a bool. Add points to the new segments to maintain shape after subdivision. New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SetSplineSettings¶
-
SubdivideSegmentBuilder.
SetSplineSettings
¶ Overloaded method SetSplineSettings
SetSplineSettings(createTangency, addPoints)
SetSplineSettings(createTangency, addPoints, addFixConstraint)
-------------------------------------
Sets options for subdividing splines.
Signature
SetSplineSettings(createTangency, addPoints)
Parameters: - createTangency (bool) – Creates tangency at the point where the spline is subdivided by adding parallel extensions.
- addPoints (bool) – Add points to the new segments to maintain shape after subdivision.
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets options for subdividing splines.
Signature
SetSplineSettings(createTangency, addPoints, addFixConstraint)
Parameters: - createTangency (bool) – Creates tangency at the point where the spline is subdivided by adding parallel extensions.
- addPoints (bool) – Add points to the new segments to maintain shape after subdivision.
- addFixConstraint (bool) – Adds a fix constraint at newly created subdivision locations
New in version NX7.5.2.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Validate¶
-
SubdivideSegmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.