SubdivideSegmentBuilderTypes Enumeration¶
NXOpen.Routing.SubdivideSegmentBuilder.Types is an alias for NXOpen.Routing.SubdivideSegmentBuilderTypes
-
class
NXOpen.Routing.
SubdivideSegmentBuilderTypes
¶ Bases:
object
Spacing method to use for subdivision.
Enum Members
Enum Member Enum Member Description AtPoint At Point EqualSegments Equal Segments ArcLengthSegments Arc Length Segments -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-