EditCharacteristicsBuilder Class¶
-
class
NXOpen.Routing.
EditCharacteristicsBuilder
¶ Bases:
NXOpen.Builder
Builder to edit required and optional characteristics of
Routing.Stock
orAssemblies.Component
as defined in the application view file.To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateEditCharacteristicsBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ReferenceObject | Returns the reference object to obtain the characteristic values |
RouteObjectCollector | Returns the routing objects to edit characteristics. |
RoutingLevel | Returns or sets the Routing Level associated with selected objects. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ApplyReferenceObjectCharx | Apply characteristics of the reference object to the selected objects. |
ClearValues | Clear the characteristic values of the selected objects. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOptionalCharacteristicsToEdit | Returns the editable Routing.CharacteristicList that contains optional characteristics common to all the selected objects. |
GetRequiredCharacteristicsToEdit | Returns the editable Routing.CharacteristicList that contains required characteristics common to all the selected objects. |
ResetValues | Reset the characteristic values of the selected objects. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReferenceObject¶
-
EditCharacteristicsBuilder.
ReferenceObject
¶ Returns the reference object to obtain the characteristic values
-------------------------------------
Getter Method
Signature
ReferenceObject
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
RouteObjectCollector¶
-
EditCharacteristicsBuilder.
RouteObjectCollector
¶ Returns the routing objects to edit characteristics.
The objects should be either
Routing.Stock
orAssemblies.Component
-------------------------------------
Getter Method
Signature
RouteObjectCollector
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
RoutingLevel¶
-
EditCharacteristicsBuilder.
RoutingLevel
¶ Returns or sets the Routing Level associated with selected objects.
-------------------------------------
Getter Method
Signature
RoutingLevel
Returns: Return type: str New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
RoutingLevel
Parameters: routeLevel (str) – New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
ApplyReferenceObjectCharx¶
-
EditCharacteristicsBuilder.
ApplyReferenceObjectCharx
¶ Apply characteristics of the reference object to the selected objects.
Signature
ApplyReferenceObjectCharx(refObject)
Parameters: refObject ( NXOpen.NXObject
) –New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
ClearValues¶
-
EditCharacteristicsBuilder.
ClearValues
¶ Clear the characteristic values of the selected objects.
Signature
ClearValues()
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
GetOptionalCharacteristicsToEdit¶
-
EditCharacteristicsBuilder.
GetOptionalCharacteristicsToEdit
¶ Returns the editable
Routing.CharacteristicList
that contains optional characteristics common to all the selected objects.Signature
GetOptionalCharacteristicsToEdit()
Returns: The characteristics to edit. Return type: NXOpen.Routing.CharacteristicList
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
GetRequiredCharacteristicsToEdit¶
-
EditCharacteristicsBuilder.
GetRequiredCharacteristicsToEdit
¶ Returns the editable
Routing.CharacteristicList
that contains required characteristics common to all the selected objects.Signature
GetRequiredCharacteristicsToEdit()
Returns: The characteristics to edit. Return type: NXOpen.Routing.CharacteristicList
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
ResetValues¶
-
EditCharacteristicsBuilder.
ResetValues
¶ Reset the characteristic values of the selected objects.
Signature
ResetValues()
New in version NX7.5.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
EditCharacteristicsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.