AssignCornerBuilder Class¶
-
class
NXOpen.Routing.
AssignCornerBuilder
¶ Bases:
NXOpen.Builder
Builder class for Assign Corner which creates corner
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateAssignCornerBuilder()
Default values.
Property Value RouteAssignCornerCornerBlock.RouteCornerBendMethods Radius RouteAssignCornerCornerBlock.RouteCornerBendOptions Radius RouteAssignCornerCornerBlock.RouteCornerRadius.Value 0 (millimeters part), 0 (inches part) RouteAssignCornerCornerBlock.RouteCornerRatioToDiameter.Value 0 (millimeters part), 0 (inches part) RouteAssignCornerCornerBlock.RouteCornerRequireLinearSolution 0 RouteAssignCornerCornerBlock.RouteCornerTypeOptions None New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ReverseValue | Returns or sets the value to store whether reverse order (for bend creation) or not |
RouteAssignCornerCornerBlock | Returns the route assign corner corner block |
RouteAssignCornerEndObject | Returns the route assign corner end objects. |
RouteAssignCornerRouteSelection | Returns the routing object colletor |
RouteAssignCornerStartObject | Returns the route assign corner start objects. |
SelectCopeStock | Returns the user selected correct object where correct object is NXOpen.Routing.Stock and NXOpen.Routing.ISegment . |
Tag | Returns the Tag for this object. |
UBendSelection | Returns the routing object collector for ubend |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAttributeHolder | Gets Attribute holder in builder, which is user for template attribute assignment. |
GetBendCornerAttributes | Corner Attributes |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetBendCornerAttributes | Corner Attributes |
SetStockList | Set the NXOpen.Routing.Stock object list when list box is updated. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReverseValue¶
-
AssignCornerBuilder.
ReverseValue
¶ Returns or sets the value to store whether reverse order (for bend creation) or not
-------------------------------------
Getter Method
Signature
ReverseValue
Returns: Return type: int New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ReverseValue
Parameters: num (int) – New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
RouteAssignCornerCornerBlock¶
-
AssignCornerBuilder.
RouteAssignCornerCornerBlock
¶ Returns the route assign corner corner block
-------------------------------------
Getter Method
Signature
RouteAssignCornerCornerBlock
Returns: Return type: NXOpen.Routing.CornerTypeBuilder
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
RouteAssignCornerEndObject¶
-
AssignCornerBuilder.
RouteAssignCornerEndObject
¶ Returns the route assign corner end objects.
Valid start objects objects are
NXOpen.Routing.ControlPoint
andNXOpen.Routing.ISegment
-------------------------------------
Getter Method
Signature
RouteAssignCornerEndObject
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
RouteAssignCornerRouteSelection¶
-
AssignCornerBuilder.
RouteAssignCornerRouteSelection
¶ Returns the routing object colletor
-------------------------------------
Getter Method
Signature
RouteAssignCornerRouteSelection
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
RouteAssignCornerStartObject¶
-
AssignCornerBuilder.
RouteAssignCornerStartObject
¶ Returns the route assign corner start objects.
Valid start objects are
NXOpen.Routing.ControlPoint
andNXOpen.Routing.ISegment
-------------------------------------
Getter Method
Signature
RouteAssignCornerStartObject
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
SelectCopeStock¶
-
AssignCornerBuilder.
SelectCopeStock
¶ Returns the user selected correct object where correct object is
NXOpen.Routing.Stock
andNXOpen.Routing.ISegment
.-------------------------------------
Getter Method
Signature
SelectCopeStock
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
UBendSelection¶
-
AssignCornerBuilder.
UBendSelection
¶ Returns the routing object collector for ubend
-------------------------------------
Getter Method
Signature
UBendSelection
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
GetAttributeHolder¶
-
AssignCornerBuilder.
GetAttributeHolder
¶ Gets Attribute holder in builder, which is user for template attribute assignment.
Signature
GetAttributeHolder()
Returns: Object to hold template attributes Return type: NXOpen.NXObject
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
GetBendCornerAttributes¶
-
AssignCornerBuilder.
GetBendCornerAttributes
¶ Corner Attributes
Signature
GetBendCornerAttributes()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
SetBendCornerAttributes¶
-
AssignCornerBuilder.
SetBendCornerAttributes
¶ Corner Attributes
Signature
SetBendCornerAttributes(selectedRowAttributesCharxList)
Parameters: selectedRowAttributesCharxList ( NXOpen.Routing.CharacteristicList
) –New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
SetStockList¶
-
AssignCornerBuilder.
SetStockList
¶ Set the
NXOpen.Routing.Stock
object list when list box is updated.Signature
SetStockList(stockObjects)
Parameters: stockObjects (list of NXOpen.Routing.Stock
) – Routing Stocks for cope creationNew in version NX8.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
AssignCornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.