CommandLibrary Class¶
-
class
NXOpen.Report.
CommandLibrary
¶ Bases:
NXOpen.TaggedObject
,NXOpen.INXObject
Represents a command library in the command manager.
Not support KF.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetCommands | Gets all commands in command library. |
MoveCommands | Moves the commands to the new position. |
Prints a representation of this object to the system log file. | |
Save | Saves all commands to their binding xml file. |
SetName | Sets the custom name of the object. |
Enumerations¶
CommandLibraryMoveCommandLocation Enumeration | Represents the moving command location. |
Property Detail¶
IsOccurrence¶
-
CommandLibrary.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CommandLibrary.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CommandLibrary.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CommandLibrary.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CommandLibrary.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CommandLibrary.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
CommandLibrary.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCommands¶
-
CommandLibrary.
GetCommands
¶ Gets all commands in command library.
Signature
GetCommands()
Returns: Return type: list of NXOpen.Report.Command
New in version NX11.0.0.
License requirements: None.
MoveCommands¶
-
CommandLibrary.
MoveCommands
¶ Moves the commands to the new position.
Signature
MoveCommands(pCommand, newLocation, pReferenceCommand)
Parameters: - pCommand (list of
NXOpen.Report.Command
) – - newLocation (
NXOpen.Report.CommandLibraryMoveCommandLocation
) – - pReferenceCommand (
NXOpen.Report.Command
) –
New in version NX11.0.0.
License requirements: None.
- pCommand (list of
Print¶
-
CommandLibrary.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
Save¶
-
CommandLibrary.
Save
¶ Saves all commands to their binding xml file.
Signature
Save()
New in version NX11.0.0.
License requirements: None.
SetName¶
-
CommandLibrary.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.