CommandLibraryMoveCommandLocation Enumeration¶
NXOpen.Report.CommandLibrary.MoveCommandLocation is an alias for NXOpen.Report.CommandLibraryMoveCommandLocation
-
class
NXOpen.Report.
CommandLibraryMoveCommandLocation
¶ Bases:
object
Represents the moving command location.
Enum Members
Enum Member Enum Member Description Before Move commands ahead of a referenced command After Move commands behind a referenced command -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-