BeginAssemblyConstraints |
Begins a mode of operation where (1) each new NXOpen.Positioning.Constraint created by this NXOpen.Positioning.ComponentPositioner applies to components in the part of the positioner (or to components with variable component positioning defined in the part of the positioner) and (2) and component transforms derived from a NXOpen.Positioning.Network will apply to components in the part of the positioner. |
BeginMoveComponent |
Begins a mode of operation where (1) each new NXOpen.Positioning.Constraint is created as transient and (2) a component transform is applied at the level where position is controlled for the component, typically in the component’s immediate parent. |
BeginMoveComponentInWorkset |
Begins a mode of operation where (1) each new NXOpen.Positioning.Constraint is created as transient and (2) a component transform is applied at the workset level. |
ClearNetwork |
Removes the NXOpen.Positioning.Network of the positioner. |
CreateAttributeIterator |
Create an attribute iterator |
CreateConstraint |
Creates a new NXOpen.Positioning.Constraint in the positioner. |
DeleteAllAttributesByType |
Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle |
Deletes an attribute by type and title. |
DeleteNonPersistentConstraints |
Deletes all the non-persistent :py:class:`NXOpen.Positioning.Constraint`s of the positioner. |
DeleteUserAttribute |
Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes |
Deletes the attributes on the object, if any, that satisfy the given iterator |
EndAssemblyConstraints |
Ends the mode of operation started by NXOpen.Positioning.ComponentPositioner.BeginAssemblyConstraints() All non-persistent constraints in this NXOpen.Positioning.ComponentPositioner will be deleted. |
EndMoveComponent |
Ends the mode of operation started by NXOpen.Positioning.ComponentPositioner.BeginMoveComponent() All constraints created while in that mode will be deleted. |
EndMoveComponentInWorkset |
Ends the mode of operation started by NXOpen.Positioning.ComponentPositioner.BeginMoveComponentInWorkset() All constraints created while in that mode will be deleted. |
EstablishNetwork |
Establishes a NXOpen.Positioning.Network in the positioner. |
FindObject |
Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType |
Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute |
Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute |
Gets a time attribute by Title and array Index. |
GetIntegerAttribute |
Gets an integer attribute by title. |
GetIntegerUserAttribute |
Gets an integer attribute by Title and array Index. |
GetNextUserAttribute |
Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue |
Gets the value of PDM Reference attribute for given object. |
GetRealAttribute |
Gets a real attribute by title. |
GetRealUserAttribute |
Gets a real attribute by Title and array Index. |
GetReferenceAttribute |
Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute |
Gets a string attribute value by title. |
GetStringUserAttribute |
Gets a string attribute by Title and array Index. |
GetTimeAttribute |
Gets a time attribute by title. |
GetTimeUserAttribute |
Gets a time attribute by Title and array Index. |
GetUserAttribute |
Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString |
Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount |
Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock |
Determine the lock of the given attribute. |
GetUserAttributeSize |
Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects |
Returns an array of objects from which this object presents attributes. |
GetUserAttributes |
Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings |
Gets all the attributes that have been set on the given object. |
HasUserAttribute |
Determines if an attribute exists on the object, that satisfies the given iterator |
LoadConstraintGeometry |
Attempts to load all the parts that contain unloaded geometry that is referenced by the constraints or by any related constraints. |
Print |
Prints a representation of this object to the system log file. |
SetAttribute |
Creates or modifies an integer attribute. |
SetBooleanUserAttribute |
Creates or modifies a boolean attribute with the option to update or not. |
SetName |
Sets the custom name of the object. |
SetPdmReferenceAttribute |
Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute |
Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute |
Creates or modifies a time attribute. |
SetTimeUserAttribute |
Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute |
Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock |
Lock or unlock the given attribute. |
SolvePostponedConstraints |
Solves constraints in all arrangements that are currently postponing their solve. |