DesignElementRevision Class¶
-
class
NXOpen.PDM.
DesignElementRevision
¶ Bases:
NXOpen.PDM.ModelElementRevision
Represents the design element revision in the database.
An instance of this class can be obtained from the
NXOpen.Assemblies.Component
.Instance of this class can not be created
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Category | Returns the category for design element. |
DesignPart | Returns the part of the underlying design element. |
EffectivityFormula | Returns the formula string that represents the effectivity of this object in database. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Modified | Returns whether the selected NXOpen.PDM.DesignElementRevision is modified in the session. |
Name | Returns the custom name of the object. |
OwningCollaborativeDesign | Returns the owning NXOpen.CollaborativeDesign . |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Create | Creates an attribute group for a NXOpen.PDM.IAttributeGroupOwner , based on an attribute group type. |
CreateAttributeGroupReviseBuilder | Creates a NXOpen.PDM.AttributeGroupReviseBuilder object. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeGroupDescriptions | Returns the NXOpen.PDM.AttributeGroupDescription objects representing the attribute group types supported by this object. |
GetAttributeGroups | Returns the NXOpen.PDM.AttributeGroup objects owned by this object. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDesignSubordinateRevisions | Get the immediate child NXOpen.PDM.DesignSubordinateRevision objects. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMemberPartitions | Get all the partitions of this model element revision. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetOverridePart | Get the override part of this model element revision if it has any. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetPositionStatus | Gets positioning status of design element. |
GetPositioningGroups | Gets all positioning group which are associated with this design element. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetTransform | Get the transform. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
IsAbsolutelyPositioned | Determine whether this design element is absolutely positioned or not. |
IsExcludedFromSpatialSearch | Determines whether this model element revision is excluded from spatial search. |
IsMemberOfPositioningGroup | Determine whether this design element is part of positioning group or not. |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetExcludeFromSpatialSearch | Set or unset this model element revision from exclusion from spatial search. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
DesignElementRevisionDesignElementCategory Enumeration | Represents the category for this design element revision. |
Property Detail¶
Category¶
-
DesignElementRevision.
Category
¶ Returns the category for design element.
Category can be unknown if the design element is new and does not yet exist in database.
-------------------------------------
Getter Method
Signature
Category
Returns: Return type: NXOpen.PDM.DesignElementRevisionDesignElementCategory
New in version NX8.5.0.
License requirements: None.
DesignPart¶
-
DesignElementRevision.
DesignPart
¶ Returns the part of the underlying design element.
This can be None for a promissory design element.
-------------------------------------
Getter Method
Signature
DesignPart
Returns: Return type: NXOpen.Part
New in version NX8.5.0.
License requirements: None.
IsOccurrence¶
-
DesignElementRevision.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DesignElementRevision.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Modified¶
-
DesignElementRevision.
Modified
¶ Returns whether the selected
NXOpen.PDM.DesignElementRevision
is modified in the session.-------------------------------------
Getter Method
Signature
Modified
Returns: Whether the selected NXOpen.PDM.DesignElementRevision
is modifiedin the session. :rtype: bool
New in version NX8.5.3.
License requirements: None.
Name¶
-
DesignElementRevision.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
DesignElementRevision.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DesignElementRevision.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
DesignElementRevision.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
Create¶
-
DesignElementRevision.
Create
¶ Creates an attribute group for a
NXOpen.PDM.IAttributeGroupOwner
, based on an attribute group type.An attribute group type is represented by an
NXOpen.PDM.AttributeGroupDescription
.Signature
Create(attributeGroupDescription)
Parameters: attributeGroupDescription ( NXOpen.PDM.AttributeGroupDescription
) –Returns: The new attribute group. Return type: NXOpen.PDM.AttributeGroup
New in version NX9.0.0.
License requirements: None.
CreateAttributeGroupReviseBuilder¶
-
DesignElementRevision.
CreateAttributeGroupReviseBuilder
¶ Overloaded method CreateAttributeGroupReviseBuilder
CreateAttributeGroupReviseBuilder(attributeGroups)
CreateAttributeGroupReviseBuilder(attributeGroups, keepOriginal, saveAsActionType)
-------------------------------------
Creates a
NXOpen.PDM.AttributeGroupReviseBuilder
object. The builder creates a revision for each attribute group in the input list of existing attribute groups.Signature
CreateAttributeGroupReviseBuilder(attributeGroups)
Parameters: attributeGroups (list of NXOpen.PDM.AttributeGroup
) –Returns: Return type: NXOpen.PDM.AttributeGroupReviseBuilder
New in version NX9.0.0.
License requirements: None.
-------------------------------------
The builder will do a revise or save-as operation for each attribute group in the input list of existing attribute groups depending on input operation type.
Signature
CreateAttributeGroupReviseBuilder(attributeGroups, keepOriginal, saveAsActionType)
Parameters: - attributeGroups (list of
NXOpen.PDM.AttributeGroup
) – - keepOriginal (bool) –
- saveAsActionType (
NXOpen.PDM.AttributeGroupReviseBuilderSaveAsActionType
) –
Returns: Return type: New in version NX11.0.0.
License requirements: None.
-------------------------------------
FindObject¶
-
DesignElementRevision.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAttributeGroupDescriptions¶
-
DesignElementRevision.
GetAttributeGroupDescriptions
¶ Returns the
NXOpen.PDM.AttributeGroupDescription
objects representing the attribute group types supported by this object.Signature
GetAttributeGroupDescriptions()
Returns: Return type: list of NXOpen.PDM.AttributeGroupDescription
New in version NX9.0.0.
License requirements: None.
GetAttributeGroups¶
-
DesignElementRevision.
GetAttributeGroups
¶ Returns the
NXOpen.PDM.AttributeGroup
objects owned by this object.Signature
GetAttributeGroups()
Returns: Return type: list of NXOpen.PDM.AttributeGroup
New in version NX9.0.0.
License requirements: None.
GetDesignSubordinateRevisions¶
-
DesignElementRevision.
GetDesignSubordinateRevisions
¶ Get the immediate child
NXOpen.PDM.DesignSubordinateRevision
objects.This will return None.for non subordinate design element.
Signature
GetDesignSubordinateRevisions()
Returns: Return type: list of NXOpen.PDM.DesignSubordinateRevision
New in version NX8.5.0.
License requirements: None.
GetTransform¶
-
DesignElementRevision.
GetTransform
¶ Get the transform.
Note: The translation component is in meters.
Signature
GetTransform()
Returns: a tuple Return type: A tuple consisting of (orientation, positionInMeters). orientation is a NXOpen.Matrix3x3
. positionInMeters is aNXOpen.Point3d
.New in version NX8.5.0.
License requirements: None.
Print¶
-
DesignElementRevision.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
DesignElementRevision.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.