AttributeGroupReviseBuilderSaveAsActionType Enumeration

NXOpen.PDM.AttributeGroupReviseBuilder.SaveAsActionType is an alias for NXOpen.PDM.AttributeGroupReviseBuilderSaveAsActionType

class NXOpen.PDM.AttributeGroupReviseBuilderSaveAsActionType

Bases: object

Represents the save as action on a managed attribute group

Enum Members

Enum Member Enum Member Description
NewRevision
NewAttributeGroup
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.