DesignStudyBuilder Class¶
-
class
NXOpen.Optimization.
DesignStudyBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Optimization.DesignStudyBuilder
To create a new instance of this class, use
NXOpen.Optimization.DesignStudyCollection.CreateDesignStudyBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
IsShowGraph | Returns or sets the property - is show graph |
IsUpdateDisp | Returns or sets the property - is update display |
StudyName | Returns or sets the study name which is unique in one part |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
BuildAllObjectives | Build all the objectives |
BuildAllVariables | Build all the variables |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDesignStudyObjectives | Returns the objectives |
GetDesignStudyVariables | Returns the variables |
GetObject | Returns the object currently being edited by this builder. |
RemoveAllObjectives | Remove all the objectives |
RemoveAllVariables | Remove all the variables |
RunDesignStudy | Run design study process |
SetDesignStudyObjectives | Sets the objectives |
SetDesignStudyVariables | Sets the variables |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DesignStudyBuilderDesignStudyAttributeType Enumeration | Attribute type |
DesignStudyBuilderDesignStudyConstraintLimitType Enumeration | Constraint limit type |
DesignStudyBuilderDesignStudyDistributeType Enumeration | Distribution type |
Structs¶
DesignStudyBuilderDesignStudyObjective_Struct Struct | Defined Objective Structure |
DesignStudyBuilderDesignStudyVariable_Struct Struct | Defined variable structure |
Property Detail¶
IsShowGraph¶
-
DesignStudyBuilder.
IsShowGraph
¶ Returns or sets the property - is show graph
-------------------------------------
Getter Method
Signature
IsShowGraph
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsShowGraph
Parameters: isShowGraph (bool) – New in version NX6.0.0.
License requirements: None.
IsUpdateDisp¶
-
DesignStudyBuilder.
IsUpdateDisp
¶ Returns or sets the property - is update display
-------------------------------------
Getter Method
Signature
IsUpdateDisp
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsUpdateDisp
Parameters: isUpdateDisp (bool) – New in version NX6.0.0.
License requirements: None.
StudyName¶
-
DesignStudyBuilder.
StudyName
¶ Returns or sets the study name which is unique in one part
-------------------------------------
Getter Method
Signature
StudyName
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StudyName
Parameters: studyName (str) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
BuildAllObjectives¶
-
DesignStudyBuilder.
BuildAllObjectives
¶ Build all the objectives
Signature
BuildAllObjectives()
New in version NX6.0.0.
License requirements: None.
BuildAllVariables¶
-
DesignStudyBuilder.
BuildAllVariables
¶ Build all the variables
Signature
BuildAllVariables()
New in version NX6.0.0.
License requirements: None.
GetDesignStudyObjectives¶
-
DesignStudyBuilder.
GetDesignStudyObjectives
¶ Returns the objectives
Signature
GetDesignStudyObjectives()
Returns: Objectives Return type: list of NXOpen.Optimization.DesignStudyBuilderDesignStudyObjective_Struct
New in version NX6.0.0.
License requirements: None.
GetDesignStudyVariables¶
-
DesignStudyBuilder.
GetDesignStudyVariables
¶ Returns the variables
Signature
GetDesignStudyVariables()
Returns: Variables Return type: list of NXOpen.Optimization.DesignStudyBuilderDesignStudyVariable_Struct
New in version NX6.0.0.
License requirements: None.
RemoveAllObjectives¶
-
DesignStudyBuilder.
RemoveAllObjectives
¶ Remove all the objectives
Signature
RemoveAllObjectives()
New in version NX6.0.0.
License requirements: None.
RemoveAllVariables¶
-
DesignStudyBuilder.
RemoveAllVariables
¶ Remove all the variables
Signature
RemoveAllVariables()
New in version NX6.0.0.
License requirements: None.
RunDesignStudy¶
-
DesignStudyBuilder.
RunDesignStudy
¶ Run design study process
Signature
RunDesignStudy()
New in version NX6.0.0.
License requirements: None.
SetDesignStudyObjectives¶
-
DesignStudyBuilder.
SetDesignStudyObjectives
¶ Sets the objectives
Signature
SetDesignStudyObjectives(attributeNames, attributeObjects, objectiveTypes, warningLowerLimit, warningUpperLimit, failureLowerLimit, failureUpperLimit)
Parameters: - attributeNames (list of str) – Objective attribute name array
- attributeObjects (list of
NXOpen.NXObject
) – Objective attribute object array - objectiveTypes (list of
NXOpen.Optimization.DesignStudyBuilderDesignStudyAttributeType
) – Objective attribute type array - warningLowerLimit (list of float) – Warning lower limit
- warningUpperLimit (list of float) – Warning upper limit
- failureLowerLimit (list of float) – Failure lower limit
- failureUpperLimit (list of float) – Failure upper limit
New in version NX6.0.0.
License requirements: None.
SetDesignStudyVariables¶
-
DesignStudyBuilder.
SetDesignStudyVariables
¶ Sets the variables
Signature
SetDesignStudyVariables(attributeNames, attributeObjects, variableTypes, variableLowerLimitValue, variableUpperLimitValue, distributeType, locationParameter, scaleParameter, shapeParameter, valuesCount)
Parameters: - attributeNames (list of str) – Variable attribute name array
- attributeObjects (list of
NXOpen.NXObject
) – Variable attribute object array - variableTypes (list of
NXOpen.Optimization.DesignStudyBuilderDesignStudyAttributeType
) – Variable attribute type array - variableLowerLimitValue (list of float) – Variable lower limit value array
- variableUpperLimitValue (list of float) – Variable upper limit value array
- distributeType (list of
NXOpen.Optimization.DesignStudyBuilderDesignStudyDistributeType
) – Distribute type - locationParameter (list of float) – Location parameter
- scaleParameter (list of float) – Scale parameter
- shapeParameter (list of float) – Shape parameter
- valuesCount (list of int) – Values count
New in version NX6.0.0.
License requirements: None.
Validate¶
-
DesignStudyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.