AddSubmechanismBuilder Class¶
-
class
NXOpen.Motion.
AddSubmechanismBuilder
¶ Bases:
NXOpen.Builder
,NXOpen.IAttributeSourceObjectBuilder
Represents a builder class that performs add submechanism in current context.
To create a new instance of this class, use
NXOpen.Motion.MotionSimulation.CreateAddSubmechanismBuilder()
Default values.
Property Value LayerOption Original UserLayer 1 New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
LayerOption | Returns or sets the layers to which geometry are added |
SelectedPart | Returns or sets the Motion Simulation part to add as sumbechanism |
Tag | Returns the Tag for this object. |
UserLayer | Returns or sets the user defined layer (should be a value in the range 1-256) |
Methods¶
Method | Description |
---|---|
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
AutoAssignAttributesWithNamingPattern | Auto assigns the attributes for a given object and returns an array of objects that failed to auto assign. |
Commit | Commits any edits that have been applied to the builder. |
CreateAttributeTitleToNamingPatternMap | Creates a map object of attribute titles to their corresponding naming pattern |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AddSubmechanismBuilderLayer Enumeration | Represents initial location type that can be present during add component |
Property Detail¶
LayerOption¶
-
AddSubmechanismBuilder.
LayerOption
¶ Returns or sets the layers to which geometry are added
-------------------------------------
Getter Method
Signature
LayerOption
Returns: Return type: NXOpen.Motion.AddSubmechanismBuilderLayer
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayerOption
Parameters: layerOption ( NXOpen.Motion.AddSubmechanismBuilderLayer
) –New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
SelectedPart¶
-
AddSubmechanismBuilder.
SelectedPart
¶ Returns or sets the Motion Simulation part to add as sumbechanism
-------------------------------------
Getter Method
Signature
SelectedPart
Returns: Return type: NXOpen.NXObject
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedPart
Parameters: part ( NXOpen.NXObject
) –New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
UserLayer¶
-
AddSubmechanismBuilder.
UserLayer
¶ Returns or sets the user defined layer (should be a value in the range 1-256)
-------------------------------------
Getter Method
Signature
UserLayer
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserLayer
Parameters: layer (int) – New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
AutoAssignAttributes¶
-
AddSubmechanismBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
AutoAssignAttributesWithNamingPattern¶
-
AddSubmechanismBuilder.
AutoAssignAttributesWithNamingPattern
¶ Auto assigns the attributes for a given object and returns an array of objects that failed to auto assign.
properties needs to be created using
CreateAttributeTitleToNamingPatternMap()
Signature
AutoAssignAttributesWithNamingPattern(objects, properties)
Parameters: - objects (list of
NXOpen.NXObject
) – - properties (list of
NXOpen.NXObject
) –
Returns: Return type: New in version NX12.0.0.
License requirements: None.
- objects (list of
CreateAttributeTitleToNamingPatternMap¶
-
AddSubmechanismBuilder.
CreateAttributeTitleToNamingPatternMap
¶ Creates a map object of attribute titles to their corresponding naming pattern
Signature
CreateAttributeTitleToNamingPatternMap(attributeTitles, titlePatterns)
Parameters: - attributeTitles (list of str) –
- titlePatterns (list of str) –
Returns: Return type: New in version NX12.0.0.
License requirements: None.
Validate¶
-
AddSubmechanismBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.