AddSubmechanismBuilderLayer Enumeration¶
NXOpen.Motion.AddSubmechanismBuilder.Layer is an alias for NXOpen.Motion.AddSubmechanismBuilderLayer
-
class
NXOpen.Motion.
AddSubmechanismBuilderLayer
¶ Bases:
object
Represents initial location type that can be present during add component
Enum Members
Enum Member Enum Member Description Original the original layer Work the work laye Specified custom specified layer -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-