PneumaticValveBuilder Class¶
-
class
NXOpen.Mechatronics.
PneumaticValveBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.PneumaticValve
builder.To create a new instance of this class, use
NXOpen.Mechatronics.PneumaticValveCollection.CreatePneumaticValveBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ControlInput | Returns the initial control input. |
Cylinders | Returns the Cylinders. This can be a PneumaticCylinder . |
ExhaustPressure | Returns the initial exhaust pressure. |
Name | Returns or sets the name. |
NominalFlow | Returns the initial nominal flow. |
NominalPressure | Returns the initial nominal pressure. |
SupplyPressure | Returns the initial supply pressure. |
Tag | Returns the Tag for this object. |
ValveType | Returns or sets the valve type. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetCylinders | the Cylinders. Sets the cylinder array. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PneumaticValveBuilderOutputValveType Enumeration | the Valve types. |
Property Detail¶
ControlInput¶
-
PneumaticValveBuilder.
ControlInput
¶ Returns the initial control input.
-------------------------------------
Getter Method
Signature
ControlInput
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Cylinders¶
-
PneumaticValveBuilder.
Cylinders
¶ Returns the Cylinders. This can be a
PneumaticCylinder
.-------------------------------------
Getter Method
Signature
Cylinders
Returns: Return type: NXOpen.Mechatronics.SelectPneumaticCylinderList
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ExhaustPressure¶
-
PneumaticValveBuilder.
ExhaustPressure
¶ Returns the initial exhaust pressure.
-------------------------------------
Getter Method
Signature
ExhaustPressure
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
NominalFlow¶
-
PneumaticValveBuilder.
NominalFlow
¶ Returns the initial nominal flow.
-------------------------------------
Getter Method
Signature
NominalFlow
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
NominalPressure¶
-
PneumaticValveBuilder.
NominalPressure
¶ Returns the initial nominal pressure.
-------------------------------------
Getter Method
Signature
NominalPressure
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SupplyPressure¶
-
PneumaticValveBuilder.
SupplyPressure
¶ Returns the initial supply pressure.
-------------------------------------
Getter Method
Signature
SupplyPressure
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ValveType¶
-
PneumaticValveBuilder.
ValveType
¶ Returns or sets the valve type.
-------------------------------------
Getter Method
Signature
ValveType
Returns: Return type: NXOpen.Mechatronics.PneumaticValveBuilderOutputValveType
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ValveType
Parameters: valveType ( NXOpen.Mechatronics.PneumaticValveBuilderOutputValveType
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetCylinders¶
-
PneumaticValveBuilder.
SetCylinders
¶ the Cylinders. Sets the cylinder array.
Signature
SetCylinders(cylinders)
Parameters: cylinders (list of NXOpen.Mechatronics.PneumaticCylinder
) – Input geometriesNew in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
PneumaticValveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.