PneumaticValveCollection Class¶
-
class
NXOpen.Mechatronics.
PneumaticValveCollection
¶ Bases:
object
Represents a collection of Pneumatic Valve.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreatePneumaticValveBuilder | Creates a NXOpen.Mechatronics.PneumaticValveBuilder . |
FindObject | Finds the NXOpen.Mechatronics.PneumaticValve with the given name. An exception will be thrown if no object can be found with given name. |
Method Detail¶
CreatePneumaticValveBuilder¶
-
PneumaticValveCollection.
CreatePneumaticValveBuilder
¶ Creates a
NXOpen.Mechatronics.PneumaticValveBuilder
.Signature
CreatePneumaticValveBuilder(pneumaticValve)
Parameters: pneumaticValve ( NXOpen.Mechatronics.PneumaticValve
) –NXOpen.Mechatronics.PneumaticValve
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.PneumaticValveBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
PneumaticValveCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.PneumaticValve
with the given name. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.PneumaticValve
.Returns: NXOpen.Mechatronics.PneumaticValve
with this name.Return type: NXOpen.Mechatronics.PneumaticValve
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)