PneumaticValveBuilderOutputValveType Enumeration¶
NXOpen.Mechatronics.PneumaticValveBuilder.OutputValveType is an alias for NXOpen.Mechatronics.PneumaticValveBuilderOutputValveType
-
class
NXOpen.Mechatronics.
PneumaticValveBuilderOutputValveType
¶ Bases:
object
the Valve types.
Enum Members
Enum Member Enum Member Description FourWay 4-way valve ThreeWay 3-way valve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-