MCDSignalServerConfigurationBuilder Class¶
-
class
NXOpen.Mechatronics.
MCDSignalServerConfigurationBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.MCDSignalServerConfigurationBuilder
It is used to maintain all server builders for MCD signals. Such as SHM, TCP/UDP, etc.
To create a new instance of this class, use
NXOpen.Mechatronics.MCDSignalServerConfigurationCollection.CreateMCDSignalServerConfigurationBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
SHMSignalProvider | Returns the SHMSignalProviderBuilder that holds the configuration for SHMSignalProvider. |
TCPSignalServer | Returns the TCPSignalServerBuilder that holds the configuration for TCPSignalServer. |
Tag | Returns the Tag for this object. |
UDPSignalServer | Returns the UDPSignalServer builder that holds the configuration for UDPSignalServer. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SHMSignalProvider¶
-
MCDSignalServerConfigurationBuilder.
SHMSignalProvider
¶ Returns the SHMSignalProviderBuilder that holds the configuration for SHMSignalProvider.
-------------------------------------
Getter Method
Signature
SHMSignalProvider
Returns: Return type: NXOpen.Mechatronics.SHMSignalProviderBuilder
New in version NX12.0.0.
License requirements: None.
TCPSignalServer¶
-
MCDSignalServerConfigurationBuilder.
TCPSignalServer
¶ Returns the TCPSignalServerBuilder that holds the configuration for TCPSignalServer.
-------------------------------------
Getter Method
Signature
TCPSignalServer
Returns: Return type: NXOpen.Mechatronics.TCPSignalServerBuilder
New in version NX12.0.0.
License requirements: None.
UDPSignalServer¶
-
MCDSignalServerConfigurationBuilder.
UDPSignalServer
¶ Returns the UDPSignalServer builder that holds the configuration for UDPSignalServer.
-------------------------------------
Getter Method
Signature
UDPSignalServer
Returns: Return type: NXOpen.Mechatronics.UDPSignalServerBuilder
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MCDSignalServerConfigurationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.