SHMSignalProviderBuilder Class¶
-
class
NXOpen.Mechatronics.
SHMSignalProviderBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.SHMSignalProviderBuilder
This class is sub-object of another builder, and cannot be directly instantiated.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
CreateShm | Returns or sets get the Ceate SHM toggle status. |
IsLittleEndian | Returns or sets the endian type. |
ShmMutex | Returns or sets ge the SHM Mutex. |
ShmName | Returns or sets get the SHM Name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSHMSignals | Get SHMProvider Signals Infomation |
SetSHMSignals | Set SHMProvider Signals Infomation |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Structs¶
SHMSignalProviderBuilderSignalInfo_Struct Struct |
|
Property Detail¶
CreateShm¶
-
SHMSignalProviderBuilder.
CreateShm
¶ Returns or sets get the Ceate SHM toggle status.
-------------------------------------
Getter Method
Signature
CreateShm
Returns: Return type: bool New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
CreateShm
Parameters: createSHM (bool) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
IsLittleEndian¶
-
SHMSignalProviderBuilder.
IsLittleEndian
¶ Returns or sets the endian type.
-------------------------------------
Getter Method
Signature
IsLittleEndian
Returns: Return type: bool New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
IsLittleEndian
Parameters: isLittleEndian (bool) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ShmMutex¶
-
SHMSignalProviderBuilder.
ShmMutex
¶ Returns or sets ge the SHM Mutex.
-------------------------------------
Getter Method
Signature
ShmMutex
Returns: Return type: str New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ShmMutex
Parameters: shmmutex (str) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ShmName¶
-
SHMSignalProviderBuilder.
ShmName
¶ Returns or sets get the SHM Name.
-------------------------------------
Getter Method
Signature
ShmName
Returns: Return type: str New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ShmName
Parameters: name (str) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
GetSHMSignals¶
-
SHMSignalProviderBuilder.
GetSHMSignals
¶ Get SHMProvider Signals Infomation
Signature
GetSHMSignals()
Returns: Array of SignalInfos Return type: list of NXOpen.Mechatronics.SHMSignalProviderBuilderSignalInfo_Struct
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetSHMSignals¶
-
SHMSignalProviderBuilder.
SetSHMSignals
¶ Set SHMProvider Signals Infomation
Signature
SetSHMSignals(signalInfos)
Parameters: signalInfos (list of NXOpen.Mechatronics.SHMSignalProviderBuilderSignalInfo_Struct
) – Array of SignalInfosNew in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
SHMSignalProviderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.