MCDSignalServerConfigurationCollection Class¶
-
class
NXOpen.Mechatronics.
MCDSignalServerConfigurationCollection
¶ Bases:
object
Represents a collection of MCDSignalServerConfigurationObject.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateMCDSignalServerConfigurationBuilder | Creates a NXOpen.Mechatronics.MCDSignalServerConfigurationBuilder . |
FindObject | Finds the NXOpen.Mechatronics.MCDSignalServerConfigurationObject with the given name. An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with given name. |
Method Detail¶
CreateMCDSignalServerConfigurationBuilder¶
-
MCDSignalServerConfigurationCollection.
CreateMCDSignalServerConfigurationBuilder
¶ Creates a
NXOpen.Mechatronics.MCDSignalServerConfigurationBuilder
.Signature
CreateMCDSignalServerConfigurationBuilder(pMCDSignalServerConfigurationObject)
Parameters: pMCDSignalServerConfigurationObject ( NXOpen.Mechatronics.MCDSignalServerConfigurationObject
) –NXOpen.Mechatronics.MCDSignalServerConfigurationObject
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.MCDSignalServerConfigurationBuilder
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
MCDSignalServerConfigurationCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.MCDSignalServerConfigurationObject
with the given name. An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals. An exception will be thrown if no object can be found with given name.Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.MCDSignalServerConfigurationObject
.Returns: NXOpen.Mechatronics.MCDSignalServerConfigurationObject
with this name.Return type: NXOpen.Mechatronics.MCDSignalServerConfigurationObject
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)