ExportToDWGBuilder Class¶
-
class
NXOpen.LineDesigner.
ExportToDWGBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.ExportToDWG
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateExportToDwgBuilder()
Default values.
Property Value MonochromeDisplay 0 SaveAs T2d TemplateSheet A0Size New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FileName | Returns or sets the file name |
FolderName | Returns or sets the folder name |
MonochromeDisplay | Returns or sets the monochrome display is return |
SaveAs | Returns or sets an API to get save as type |
Tag | Returns the Tag for this object. |
TemplateSheet | Returns or sets the template sheet type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExportToDWGBuilderSaveAsTypeAPI Enumeration | This enum represents the dwg saving types |
ExportToDWGBuilderTemplateTypeAPI Enumeration | This enum represents the dwg sheet template types |
Property Detail¶
FileName¶
-
ExportToDWGBuilder.
FileName
¶ Returns or sets the file name
-------------------------------------
Getter Method
Signature
FileName
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
FileName
Parameters: fileName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
FolderName¶
-
ExportToDWGBuilder.
FolderName
¶ Returns or sets the folder name
-------------------------------------
Getter Method
Signature
FolderName
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
FolderName
Parameters: foldername (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
MonochromeDisplay¶
-
ExportToDWGBuilder.
MonochromeDisplay
¶ Returns or sets the monochrome display is return
-------------------------------------
Getter Method
Signature
MonochromeDisplay
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
MonochromeDisplay
Parameters: monochromeDisplay (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SaveAs¶
-
ExportToDWGBuilder.
SaveAs
¶ Returns or sets an API to get save as type
-------------------------------------
Getter Method
Signature
SaveAs
Returns: Return type: NXOpen.LineDesigner.ExportToDWGBuilderSaveAsTypeAPI
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SaveAs
Parameters: saveAs ( NXOpen.LineDesigner.ExportToDWGBuilderSaveAsTypeAPI
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TemplateSheet¶
-
ExportToDWGBuilder.
TemplateSheet
¶ Returns or sets the template sheet type
-------------------------------------
Getter Method
Signature
TemplateSheet
Returns: Return type: NXOpen.LineDesigner.ExportToDWGBuilderTemplateTypeAPI
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
TemplateSheet
Parameters: templateSheet ( NXOpen.LineDesigner.ExportToDWGBuilderTemplateTypeAPI
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
ExportToDWGBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.