ExportToDWGBuilderSaveAsTypeAPI Enumeration¶
NXOpen.LineDesigner.ExportToDWGBuilder.SaveAsTypeAPI is an alias for NXOpen.LineDesigner.ExportToDWGBuilderSaveAsTypeAPI
-
class
NXOpen.LineDesigner.
ExportToDWGBuilderSaveAsTypeAPI
¶ Bases:
object
This enum represents the dwg saving types
Enum Members
Enum Member Enum Member Description T2d Represents the 2D type T3d Represents the 3D type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-