ExportToDWGBuilderTemplateTypeAPI Enumeration¶
NXOpen.LineDesigner.ExportToDWGBuilder.TemplateTypeAPI is an alias for NXOpen.LineDesigner.ExportToDWGBuilderTemplateTypeAPI
-
class
NXOpen.LineDesigner.
ExportToDWGBuilderTemplateTypeAPI
¶ Bases:
object
This enum represents the dwg sheet template types
Enum Members
Enum Member Enum Member Description A0Size Represents the A0 type A1Size Represents the A1 type A2Size Represents the A2 type A3Size Represents the A3 type A4Size Represents the A4 type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-