LineColorFontWidthBuilder Class¶
-
class
NXOpen.
LineColorFontWidthBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represent a
NXOpen.LineColorFontWidthBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
LineColor | Returns or sets the line color |
LineFont | Returns the line font |
LineWidth | Returns or sets the line width |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LineColor¶
-
LineColorFontWidthBuilder.
LineColor
¶ Returns or sets the line color
-------------------------------------
Getter Method
Signature
LineColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineColor
Parameters: lineColor (Id) – New in version NX9.0.0.
License requirements: None.
LineFont¶
-
LineColorFontWidthBuilder.
LineFont
¶ Returns the line font
-------------------------------------
Getter Method
Signature
LineFont
Returns: Return type: NXOpen.LineFontBuilder
New in version NX9.0.0.
License requirements: None.
LineWidth¶
-
LineColorFontWidthBuilder.
LineWidth
¶ Returns or sets the line width
-------------------------------------
Getter Method
Signature
LineWidth
Returns: Return type: NXOpen.DisplayableObjectObjectWidth
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineWidth
Parameters: width ( NXOpen.DisplayableObjectObjectWidth
) –New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LineColorFontWidthBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.