LineFontBuilder Class¶
-
class
NXOpen.
LineFontBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represent a
NXOpen.LineFontBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
LineFont | Returns or sets the line font |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LineFontBuilderLineFontType Enumeration | line font types |
Property Detail¶
LineFont¶
-
LineFontBuilder.
LineFont
¶ Returns or sets the line font
-------------------------------------
Getter Method
Signature
LineFont
Returns: Return type: NXOpen.LineFontBuilderLineFontType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineFont
Parameters: lineFont ( NXOpen.LineFontBuilderLineFontType
) –New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LineFontBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.