DisplayableObjectObjectWidth Enumeration¶
NXOpen.DisplayableObject.ObjectWidth is an alias for NXOpen.DisplayableObjectObjectWidth
-
class
NXOpen.
DisplayableObjectObjectWidth
¶ Bases:
object
specifies object width for objects such as lines and text
New in version NX3.0.0.
Enum Members
Enum Member Enum Member Description Normal Thick Thin One Two Three Four Five Six Seven Eight Nine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-