RectangularPattern Class¶
-
class
NXOpen.GeometricUtilities.
RectangularPattern
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
the rectangular pattern definition.
Allows specification along two linear axes, which may or may not be orthogonal. .. versionadded:: NX7.5.0
Properties¶
Property | Description |
---|---|
CreateLastStaggered | Returns or sets the option to generate the last item in a staggered row. |
HorizontalRef | Returns the horizontal reference |
SimplifiedLayoutType | Returns or sets the simplified layout type to be used by the pattern |
StaggerType | Returns or sets the type of stagger to be used by the pattern |
Tag | Returns the Tag for this object. |
UseYDirectionToggle | Returns or sets the UseYDirection toggle attribute. |
XDirection | Returns or sets the x axis |
XFlip | Returns or sets the XSelection flip attribute. |
XSelection | Returns the direction object. |
XSpacing | Returns the instance spacing along the x axis |
XSymmetryToggle | Returns or sets the XSymmetry toggle attribute. |
YDirection | Returns or sets the y axis, which can be any vector not parallel to the x axis |
YFlip | Returns or sets the YSelection flip attribute. |
YSelection | Returns the direction object. |
YSpacing | Returns the instance spacing along the y axis |
YSymmetryToggle | Returns or sets the YSymmetry toggle attribute. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RectangularPatternSimplifiedLayoutTypes Enumeration | defines simplified layout type for linear pattern. |
RectangularPatternStaggerOptions Enumeration | defines any stagger to be defined on the pattern. |
Property Detail¶
CreateLastStaggered¶
-
RectangularPattern.
CreateLastStaggered
¶ Returns or sets the option to generate the last item in a staggered row.
If ‘true’ the pattern will be narrower on rows that have been staggered.
-------------------------------------
Getter Method
Signature
CreateLastStaggered
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateLastStaggered
Parameters: create (bool) – New in version NX7.5.0.
License requirements: None.
HorizontalRef¶
-
RectangularPattern.
HorizontalRef
¶ Returns the horizontal reference
-------------------------------------
Getter Method
Signature
HorizontalRef
Returns: Return type: NXOpen.GeometricUtilities.HorizontalReference
New in version NX8.0.0.
License requirements: None.
SimplifiedLayoutType¶
-
RectangularPattern.
SimplifiedLayoutType
¶ Returns or sets the simplified layout type to be used by the pattern
-------------------------------------
Getter Method
Signature
SimplifiedLayoutType
Returns: Return type: NXOpen.GeometricUtilities.RectangularPatternSimplifiedLayoutTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SimplifiedLayoutType
Parameters: type ( NXOpen.GeometricUtilities.RectangularPatternSimplifiedLayoutTypes
) –New in version NX8.0.0.
License requirements: None.
StaggerType¶
-
RectangularPattern.
StaggerType
¶ Returns or sets the type of stagger to be used by the pattern
-------------------------------------
Getter Method
Signature
StaggerType
Returns: Return type: NXOpen.GeometricUtilities.RectangularPatternStaggerOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StaggerType
Parameters: spaceType ( NXOpen.GeometricUtilities.RectangularPatternStaggerOptions
) –New in version NX7.5.0.
License requirements: None.
UseYDirectionToggle¶
-
RectangularPattern.
UseYDirectionToggle
¶ Returns or sets the UseYDirection toggle attribute.
This function gets the UseYDirection toggle value
-------------------------------------
Getter Method
Signature
UseYDirectionToggle
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseYDirectionToggle
Parameters: toggle (bool) – New in version NX7.5.0.
License requirements: None.
XDirection¶
-
RectangularPattern.
XDirection
¶ Returns or sets the x axis
-------------------------------------
Getter Method
Signature
XDirection
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XDirection
Parameters: xDirection ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
XFlip¶
-
RectangularPattern.
XFlip
¶ Returns or sets the XSelection flip attribute.
This function flips X selection object of the 2D pattern
-------------------------------------
Getter Method
Signature
XFlip
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XFlip
Parameters: flip (bool) – New in version NX7.5.0.
License requirements: None.
XSelection¶
-
RectangularPattern.
XSelection
¶ Returns the direction object.
This function gets X direction object of the 2D pattern. This call will result in an Exception if not called in 2D mode.
-------------------------------------
Getter Method
Signature
XSelection
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: None.
XSpacing¶
-
RectangularPattern.
XSpacing
¶ Returns the instance spacing along the x axis
-------------------------------------
Getter Method
Signature
XSpacing
Returns: Return type: NXOpen.GeometricUtilities.DistancePatternSpacing
New in version NX7.5.0.
License requirements: None.
XSymmetryToggle¶
-
RectangularPattern.
XSymmetryToggle
¶ Returns or sets the XSymmetry toggle attribute.
This function gets the x Symmetry toggle value
-------------------------------------
Getter Method
Signature
XSymmetryToggle
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XSymmetryToggle
Parameters: toggle (bool) – New in version NX7.5.0.
License requirements: None.
YDirection¶
-
RectangularPattern.
YDirection
¶ Returns or sets the y axis, which can be any vector not parallel to the x axis
-------------------------------------
Getter Method
Signature
YDirection
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YDirection
Parameters: yDirection ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
YFlip¶
-
RectangularPattern.
YFlip
¶ Returns or sets the YSelection flip attribute.
This function flips Y selection object of the 2D pattern
-------------------------------------
Getter Method
Signature
YFlip
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YFlip
Parameters: flip (bool) – New in version NX7.5.0.
License requirements: None.
YSelection¶
-
RectangularPattern.
YSelection
¶ Returns the direction object.
This function gets Y direction object of the 2D pattern. This call will result in an Exception if not called in 2D mode.
-------------------------------------
Getter Method
Signature
YSelection
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: None.
YSpacing¶
-
RectangularPattern.
YSpacing
¶ Returns the instance spacing along the y axis
-------------------------------------
Getter Method
Signature
YSpacing
Returns: Return type: NXOpen.GeometricUtilities.DistancePatternSpacing
New in version NX7.5.0.
License requirements: None.
YSymmetryToggle¶
-
RectangularPattern.
YSymmetryToggle
¶ Returns or sets the YSymmetry toggle attribute.
This function gets the y Symmetry toggle value
-------------------------------------
Getter Method
Signature
YSymmetryToggle
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YSymmetryToggle
Parameters: toggle (bool) – New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
RectangularPattern.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.