HorizontalReference Class¶
-
class
NXOpen.GeometricUtilities.
HorizontalReference
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
the horizontal reference vector definition.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Flip | Returns or sets the 2D Selection flip attribute. |
HorizontalRefObject | Returns the direction object. |
HorizontalRefVector | Returns or sets the horizontal reference vector |
RotationAngle | Returns the rotation angle wrt horizontal reference direction |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Flip¶
-
HorizontalReference.
Flip
¶ Returns or sets the 2D Selection flip attribute.
This function flips the selection object of the 2D pattern
-------------------------------------
Getter Method
Signature
Flip
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Flip
Parameters: flip (bool) – New in version NX8.0.0.
License requirements: None.
HorizontalRefObject¶
-
HorizontalReference.
HorizontalRefObject
¶ Returns the direction object.
This function gets reference vector of the 2D pattern. This call will result in an Exception if not called in 2D mode.
-------------------------------------
Getter Method
Signature
HorizontalRefObject
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.0.0.
License requirements: None.
HorizontalRefVector¶
-
HorizontalReference.
HorizontalRefVector
¶ Returns or sets the horizontal reference vector
-------------------------------------
Getter Method
Signature
HorizontalRefVector
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HorizontalRefVector
Parameters: horizontalRefVector ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: None.
RotationAngle¶
-
HorizontalReference.
RotationAngle
¶ Returns the rotation angle wrt horizontal reference direction
-------------------------------------
Getter Method
Signature
RotationAngle
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HorizontalReference.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.