RectangularPatternStaggerOptions Enumeration¶
NXOpen.GeometricUtilities.RectangularPattern.StaggerOptions is an alias for NXOpen.GeometricUtilities.RectangularPatternStaggerOptions
-
class
NXOpen.GeometricUtilities.
RectangularPatternStaggerOptions
¶ Bases:
object
defines any stagger to be defined on the pattern. Stagger values are used to offset to every other row/column of the pattern.
Enum Members
Enum Member Enum Member Description NotSet No stagger applied Row Stagger row Column Stagger column -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-