PartModuleInputBuilder Class¶
-
class
NXOpen.GeometricUtilities.
PartModuleInputBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricUtilities.PartModuleInputBuilder
To create a new instance of this class, use
NXOpen.Features.PartModule.CreatePartModuleInputBuilder()
Default values.
Property Value InputReferences.ObjectType BodyCollector ModifiableGeometryOption WholeBody New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DefineSharedBodyInput | Returns or sets the shared body inputs option. |
InputReferences | Returns the part module input data |
ModifiableGeometry | Returns the faces/edges specified as modifiable geometry |
ModifiableGeometryOption | Returns or sets the Modifiable Geometry option |
SharedBodyInput | Returns the bodies for part module shared body |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PartModuleInputBuilderModifiableGeometryOptions Enumeration | the Modifiable Geometry option types |
Property Detail¶
InputReferences¶
-
PartModuleInputBuilder.
InputReferences
¶ Returns the part module input data
-------------------------------------
Getter Method
Signature
InputReferences
Returns: Return type: NXOpen.Features.PartGeometryCopyBuilder
New in version NX9.0.0.
License requirements: None.
ModifiableGeometry¶
-
PartModuleInputBuilder.
ModifiableGeometry
¶ Returns the faces/edges specified as modifiable geometry
-------------------------------------
Getter Method
Signature
ModifiableGeometry
Returns: Return type: NXOpen.ScCollectorList
New in version NX9.0.0.
License requirements: None.
ModifiableGeometryOption¶
-
PartModuleInputBuilder.
ModifiableGeometryOption
¶ Returns or sets the Modifiable Geometry option
-------------------------------------
Getter Method
Signature
ModifiableGeometryOption
Returns: Return type: NXOpen.GeometricUtilities.PartModuleInputBuilderModifiableGeometryOptions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModifiableGeometryOption
Parameters: modifiableGeometryOption ( NXOpen.GeometricUtilities.PartModuleInputBuilderModifiableGeometryOptions
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
PartModuleInputBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.