PartModuleInputBuilderModifiableGeometryOptions Enumeration¶
NXOpen.GeometricUtilities.PartModuleInputBuilder.ModifiableGeometryOptions is an alias for NXOpen.GeometricUtilities.PartModuleInputBuilderModifiableGeometryOptions
-
class
NXOpen.GeometricUtilities.
PartModuleInputBuilderModifiableGeometryOptions
¶ Bases:
object
the Modifiable Geometry option types
Enum Members
Enum Member Enum Member Description WholeBody the whole shared body will be allowed for selection inside part module Selected the faces/edges on shared body that are allowed for selection inside part module -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-