MultiTransitionLawBuilder Class¶
-
class
NXOpen.GeometricUtilities.
MultiTransitionLawBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents multiple transition law.
This class represents
NXOpen.GeometricUtilities.LawBuilderType.MultiTransition
type of law inNXOpen.GeometricUtilities.LawBuilder
. Objects of classNXOpen.GeometricUtilities.TransitionLawNodeBuilder
are used as law nodes inNXOpen.GeometricUtilities.MultiTransitionLawBuilder
. Spine definition in this class is mandatory. You can specify any number of law nodes on the spine. Minimum two law nodes are necessary to define the multi transition law along the spine. The law nodes must be specified in the parametrically increasing order in the spine direction.Depending on the law node position on the spine following transition types are supported -
Start node - All options in
NXOpen.GeometricUtilities.TransitionLawNodeBuilderTransitionType
exceptNXOpen.GeometricUtilities.TransitionLawNodeBuilderTransitionType.Unknown
End node -
NXOpen.GeometricUtilities.TransitionLawNodeBuilderTransitionType.Blend
andNXOpen.GeometricUtilities.TransitionLawNodeBuilderTransitionType.Minmax
onlyEnd node - All options in
NXOpen.GeometricUtilities.TransitionLawNodeBuilderTransitionType
may be supported. Consult the referencing class documentation to see whenNXOpen.GeometricUtilities.TransitionLawNodeBuilderTransitionType.Unknown
is not supported at a law node.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
NodeList | Returns the list of law nodes. |
Spine | Returns the spine |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateNode | Creates a new law node |
UpdateSpine | Update the builder based on current spine |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NodeList¶
-
MultiTransitionLawBuilder.
NodeList
¶ Returns the list of law nodes.
-------------------------------------
Getter Method
Signature
NodeList
Returns: Return type: NXOpen.GeometricUtilities.TransitionLawNodeBuilderList
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Spine¶
-
MultiTransitionLawBuilder.
Spine
¶ Returns the spine
-------------------------------------
Getter Method
Signature
Spine
Returns: Section object representing spine Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
CreateNode¶
-
MultiTransitionLawBuilder.
CreateNode
¶ Creates a new law node
Signature
CreateNode()
Returns: Law node Return type: NXOpen.GeometricUtilities.TransitionLawNodeBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
UpdateSpine¶
-
MultiTransitionLawBuilder.
UpdateSpine
¶ Update the builder based on current spine
Signature
UpdateSpine()
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
MultiTransitionLawBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.