LawBuilderType Enumeration¶
NXOpen.GeometricUtilities.LawBuilder.Type is an alias for NXOpen.GeometricUtilities.LawBuilderType
-
class
NXOpen.GeometricUtilities.
LawBuilderType
¶ Bases:
object
The law types
Enum Members
Enum Member Enum Member Description Constant constant law type Linear linear law type Cubic cubic law type LinearAlongSpine linear along spine law type CubicAlongSpine cubic along spine law type ByEquation by equation law type ByLawCurve by law curve law type MultiTransition multi-transition law type NonInflecting non-inflecting law type SShaped S-shaped law type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-