TransitionLawNodeBuilderTransitionType Enumeration¶
NXOpen.GeometricUtilities.TransitionLawNodeBuilder.TransitionType is an alias for NXOpen.GeometricUtilities.TransitionLawNodeBuilderTransitionType
-
class
NXOpen.GeometricUtilities.
TransitionLawNodeBuilderTransitionType
¶ Bases:
object
Represents a transition type at a law node. Transition type is a type of interpolation used to evaluate intermediate values from one law node to the next law node. The transition is applied in the direction of the spine on which the law nodes reside. Not all nodes support all types of transitions. Consult the referencing law class documentation to see which transition types are supported by which law nodes.
Enum Members
Enum Member Enum Member Description Unknown No interpolation type Constant Constant transition Linear Linear transition Blend Smooth blended transition Minmax Minimum-Maximum type transition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-