MovePoleBuilder Class¶
-
class
NXOpen.GeometricUtilities.
MovePoleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class manages the control poles movements for a surface or curve.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ControlPoleManager | Returns the control pole manager |
DegreesAndPatches | Returns the degrees and patches |
Entity | Returns or sets the entity |
MoveMethod | Returns or sets the control pole move method |
Plane | Returns or sets the plane |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the vector |
WCSDirection | Returns or sets the fixed direction |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MovePoleBuilderMoveMethodType Enumeration | Move Pole types |
MovePoleBuilderWCSDirectionType Enumeration | WCS direction |
Property Detail¶
ControlPoleManager¶
-
MovePoleBuilder.
ControlPoleManager
¶ Returns the control pole manager
-------------------------------------
Getter Method
Signature
ControlPoleManager
Returns: Return type: NXOpen.GeometricUtilities.ControlPoleManagerData
New in version NX8.5.0.
License requirements: None.
DegreesAndPatches¶
-
MovePoleBuilder.
DegreesAndPatches
¶ Returns the degrees and patches
-------------------------------------
Getter Method
Signature
DegreesAndPatches
Returns: Return type: NXOpen.GeometricUtilities.DegreesAndSegmentsOrPatchesBuilder
New in version NX8.5.0.
License requirements: None.
Entity¶
-
MovePoleBuilder.
Entity
¶ Returns or sets the entity
-------------------------------------
Getter Method
Signature
Entity
Returns: Return type: NXOpen.NXObject
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Entity
Parameters: entity ( NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: None.
MoveMethod¶
-
MovePoleBuilder.
MoveMethod
¶ Returns or sets the control pole move method
-------------------------------------
Getter Method
Signature
MoveMethod
Returns: Return type: NXOpen.GeometricUtilities.MovePoleBuilderMoveMethodType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoveMethod
Parameters: moveMethod ( NXOpen.GeometricUtilities.MovePoleBuilderMoveMethodType
) –New in version NX8.5.0.
License requirements: None.
Plane¶
-
MovePoleBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.Plane
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.Plane
) –New in version NX8.5.0.
License requirements: None.
Vector¶
-
MovePoleBuilder.
Vector
¶ Returns or sets the vector
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: None.
WCSDirection¶
-
MovePoleBuilder.
WCSDirection
¶ Returns or sets the fixed direction
-------------------------------------
Getter Method
Signature
WCSDirection
Returns: Return type: NXOpen.GeometricUtilities.MovePoleBuilderWCSDirectionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WCSDirection
Parameters: wcsDirection ( NXOpen.GeometricUtilities.MovePoleBuilderWCSDirectionType
) –New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
MovePoleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.