SlopeAnalysisBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
SlopeAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents a Slope Analysis builder.
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollectionEx.CreateSlopeAnalysisBuilder()
Default values.
Property Value DataRange.IsFixed 1 DataRange.Max 0.010000 DataRange.Middle 0.000000 DataRange.MiddleScale 0.000000 DataRange.Min -0.010000 DataRange.ZoomScale 8 DisplayMode Fringe DisplaySettings.CanShowFacet 0 DisplaySettings.ColorLegendOption Blend DisplaySettings.DisplayResolution.AngleTolerance 15.0 DisplaySettings.DisplayResolution.EdgeTolerance 0.005 DisplaySettings.DisplayResolution.FaceTolerance 0.005 DisplaySettings.DisplayResolution.Resolution Standard DisplaySettings.DisplayResolution.WidthTolerance 0.3 DisplaySettings.NumberOfColors Seven NumberOfContourLines 8 SpikeLength 25.4 (millimeters part), 1.0 (inches part) New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DataRange | Returns the slope analysis data range. |
DisplayMode | Returns or sets the display mode. |
DisplaySettings | Returns the slope analysis display settings. |
Faces | Returns the face to apply slope analysis. |
Normals | Returns the slope analysis normals. |
NumberOfContourLines | Returns or sets the number of contour lines. |
PmiPoint | Returns the point to draw labels. |
SpikeLength | Returns or sets the spike length. |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the reference vector used for slope analysis. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreatePMILabel | Create a PMI label. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StartSlopeAnalysis | Start slope analysis. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SlopeAnalysisBuilderDisplayModes Enumeration | The display type. |
Property Detail¶
DataRange¶
-
SlopeAnalysisBuilder.
DataRange
¶ Returns the slope analysis data range.
-------------------------------------
Getter Method
Signature
DataRange
Returns: Return type: NXOpen.GeometricAnalysis.FaceAnalysisDataRangeBuilder
New in version NX11.0.0.
License requirements: None.
DisplayMode¶
-
SlopeAnalysisBuilder.
DisplayMode
¶ Returns or sets the display mode.
-------------------------------------
Getter Method
Signature
DisplayMode
Returns: Return type: NXOpen.GeometricAnalysis.SlopeAnalysisBuilderDisplayModes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayMode
Parameters: displayMode ( NXOpen.GeometricAnalysis.SlopeAnalysisBuilderDisplayModes
) –New in version NX11.0.0.
License requirements: None.
DisplaySettings¶
-
SlopeAnalysisBuilder.
DisplaySettings
¶ Returns the slope analysis display settings.
-------------------------------------
Getter Method
Signature
DisplaySettings
Returns: Return type: NXOpen.GeometricAnalysis.FaceAnalysisDisplayBuilder
New in version NX11.0.0.
License requirements: None.
Faces¶
-
SlopeAnalysisBuilder.
Faces
¶ Returns the face to apply slope analysis.
-------------------------------------
Getter Method
Signature
Faces
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
Normals¶
-
SlopeAnalysisBuilder.
Normals
¶ Returns the slope analysis normals.
-------------------------------------
Getter Method
Signature
Normals
Returns: Return type: NXOpen.GeometricAnalysis.FaceAnalysisNormalsBuilder
New in version NX11.0.0.
License requirements: None.
NumberOfContourLines¶
-
SlopeAnalysisBuilder.
NumberOfContourLines
¶ Returns or sets the number of contour lines.
-------------------------------------
Getter Method
Signature
NumberOfContourLines
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfContourLines
Parameters: numberOfContourLines (int) – New in version NX11.0.0.
License requirements: None.
PmiPoint¶
-
SlopeAnalysisBuilder.
PmiPoint
¶ Returns the point to draw labels.
-------------------------------------
Getter Method
Signature
PmiPoint
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
SpikeLength¶
-
SlopeAnalysisBuilder.
SpikeLength
¶ Returns or sets the spike length.
-------------------------------------
Getter Method
Signature
SpikeLength
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpikeLength
Parameters: spikeLength (float) – New in version NX11.0.0.
License requirements: None.
Vector¶
-
SlopeAnalysisBuilder.
Vector
¶ Returns or sets the reference vector used for slope analysis.
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: None.
Method Detail¶
CreatePMILabel¶
-
SlopeAnalysisBuilder.
CreatePMILabel
¶ Create a PMI label.
Signature
CreatePMILabel(location, face)
Parameters: - location (
NXOpen.Point3d
) – the loction on the face to create a PMI label. - face (
NXOpen.DisplayableObject
) – the selected face to create a PMI label.
New in version NX11.0.0.
License requirements: None.
- location (
StartSlopeAnalysis¶
-
SlopeAnalysisBuilder.
StartSlopeAnalysis
¶ Start slope analysis.
Signature
StartSlopeAnalysis()
New in version NX11.0.0.
License requirements: None.
Validate¶
-
SlopeAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.