SlopeAnalysisBuilderDisplayModes Enumeration

NXOpen.GeometricAnalysis.SlopeAnalysisBuilder.DisplayModes is an alias for NXOpen.GeometricAnalysis.SlopeAnalysisBuilderDisplayModes

class NXOpen.GeometricAnalysis.SlopeAnalysisBuilderDisplayModes

Bases: object

The display type.

Enum Members

Enum Member Enum Member Description
Fringe
Hedgehog
ContourLines
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.