FaceAnalysisDisplayBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
FaceAnalysisDisplayBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a set of display settings used by Face Analysis.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CanShowFacet | Returns or sets the flag indicating if facets should be shown. |
ColorLegendOption | Returns or sets the color legend option. |
DisplayResolution | Returns the display resolution. |
NumberOfColors | Returns or sets the number of colors. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FaceAnalysisDisplayBuilderColorLegendOptions Enumeration | Represents color legend type in display. |
FaceAnalysisDisplayBuilderColorsOptions Enumeration | The option indicating number of colors to be used for display. |
Property Detail¶
CanShowFacet¶
-
FaceAnalysisDisplayBuilder.
CanShowFacet
¶ Returns or sets the flag indicating if facets should be shown.
-------------------------------------
Getter Method
Signature
CanShowFacet
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanShowFacet
Parameters: canShowFacet (bool) – New in version NX11.0.0.
License requirements: None.
ColorLegendOption¶
-
FaceAnalysisDisplayBuilder.
ColorLegendOption
¶ Returns or sets the color legend option.
-------------------------------------
Getter Method
Signature
ColorLegendOption
Returns: Return type: NXOpen.GeometricAnalysis.FaceAnalysisDisplayBuilderColorLegendOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorLegendOption
Parameters: colorLegendOption ( NXOpen.GeometricAnalysis.FaceAnalysisDisplayBuilderColorLegendOptions
) –New in version NX11.0.0.
License requirements: None.
DisplayResolution¶
-
FaceAnalysisDisplayBuilder.
DisplayResolution
¶ Returns the display resolution.
-------------------------------------
Getter Method
Signature
DisplayResolution
Returns: Return type: NXOpen.GeometricUtilities.DisplayResolutionBuilder
New in version NX11.0.0.
License requirements: None.
NumberOfColors¶
-
FaceAnalysisDisplayBuilder.
NumberOfColors
¶ Returns or sets the number of colors.
-------------------------------------
Getter Method
Signature
NumberOfColors
Returns: Return type: NXOpen.GeometricAnalysis.FaceAnalysisDisplayBuilderColorsOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfColors
Parameters: numberOfColors ( NXOpen.GeometricAnalysis.FaceAnalysisDisplayBuilderColorsOptions
) –New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FaceAnalysisDisplayBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.